2020-08-01 12:10 AM
2020-08-01 8:07 AM
Above -O0 many debugging related things break apart...
2020-08-01 9:44 PM
From gcc documents:
Optimize debugging experience. -Og should be the optimization level of choice for the standard edit-compile-debug cycle, offering a reasonable level of optimization while maintaining fast compilation and a good debugging experience. It is a better choice than -O0 for producing debuggable code because some compiler passes that collect debug information are disabled at -O0.
Like -O0, -Og completely disables a number of optimization passes so that individual options controlling them have no effect. Otherwise -Og enables all -O1 optimization flags except for those that may interfere with debugging
2020-08-02 12:45 AM
> ulTutoralRunTime in tasks.c has to be defined as volatile
This may be a Atollic TrueStudio specific requirement for updating their GUI FreeRTOS Task List view.
In general, no changes are required and the code works out-of-the-box when using the FreeRTOS supplied vTaskGetRunTimeStats function.
Set up an up-counting timer running at a frequency considerably higher than the FreeRTOS tick, say TIM2 at 1 MHz.
Activate in FreeRTOSConfig.h:
#define configGENERATE_RUN_TIME_STATS 1
#define configUSE_TRACE_FACILITY 1
#define configUSE_STATS_FORMATTING_FUNCTIONS 1Override the _weak defaults by implementing:
void configureTimerForRunTimeStats(void)
{
HAL_TIM_Base_Start(&htim2);
}
unsigned long getRunTimeCounterValue(void)
{
return __HAL_TIM_GET_COUNTER(&htim2);
}And now you can periodically read-out the statistics in a tasks by:
char pcWriteBuffer[256];
vTaskGetRunTimeStats(pcWriteBuffer);and send the results to an UART or other interface. You get output like
...
defaultTask 24120810 8%
IDLE 270603162 91%
Tmr Svc 58 <1%Btw: There is no need to setup an additional timer interrupt as suggested in that tutorial. That creates only overhead...
2020-08-02 3:19 PM
Even -Og optimizes out variables and does a few things, which can make debugging cumbersome. Anyway it's not what your original topic is about. The FreeRTOS doesn't need that variable to be volatile, it's only that viewing tool under specific optimization levels, that needs it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.