2019-11-29 5:16 AM
I'm working on STM32F746 Discovery try to use STemWin. I using cubeMX to gen code for cubeIDE. But i'm stuck, sprintf %f not working. It's return 0x00 and dot instead. For example
char str[32];
float a = 123.456;
sprintf(str, "%f", a);
the result
str[0] = 0x00
str[1] = 0x00
str[2] = 0x00
str[3] = 0x26 '.'
str[4] = 0x00
str[5] = 0x00
str[6] = 0x00
Then i try to test whats wrong. I tried to gen a project without freeRTOS and test sprintf %f. And it's work fine.
Then i found this http://www.nadler.com/embedded/newlibAndFreeRTOS.html
I try to follow this step.
· Exclude from all builds any current FreeRTOS heap implementation, typically something like:
· Middlewares\Third_Party\FreeRTOS\Source\portable\MemMang\heap_4.c
· Add the module
· heap_useNewlib.c
· I've provided.
· If your application needs a complete
· snprintf
·
· implementation,
· strtok
·
· , or other newlib functions requiring reentrancy support, or you're not really sure...
· Configure FreeRTOS for newlib support. In
· FreeRTOSconfig.h
· , add the line:
· #define configUSE_NEWLIB_REENTRANT 1
but it error: heap_useNewlib.c:(.text._sbrk+0x0): multiple definition of `_sbrk'
How to fix sprintf %f problem?
Solved! Go to Solution.
2019-11-29 6:36 AM
> multiple definition of `_sbrk'
So you have another instance of _sbrk somewhere else, in sysmem.c or syscalls.c. Delete it.
-- pa
2019-11-29 6:36 AM
> multiple definition of `_sbrk'
So you have another instance of _sbrk somewhere else, in sysmem.c or syscalls.c. Delete it.
-- pa
2019-11-29 6:59 AM
Thank you. You are the best. It's work now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.