2025-02-21 9:59 AM - last edited on 2025-02-21 11:48 AM by mƎALLEm
Hello,
I am configuring a project from scratch for a STM32 FreeRTOS based.
From FreeRTOS documentation:
Low priority numbers denote low priority tasks.
The idle task has priority zero (tskIDLE_PRIORITY).
2-Kernel/02-Kernel-features/01-Tasks-and-co-routines/15-Idle-task
It is possible for application tasks to share the idle task priority (tskIDLE_PRIORITY).
See the configIDLE_SHOULD_YIELD configuration parameter for information on how this behaviour can be configured.
#define tskIDLE_PRIORITY ( ( unsigned portBASE_TYPE ) 0U )
This matches with what I can see from my project debugging:
But, I don't understant why in STM32 code, in 'cmsis_os2.h', IDLE thread priority is '1' instead of '0'.
/// Priority values.
typedef enum {
osPriorityNone = 0, ///< No priority (not initialized).
osPriorityIdle = 1, ///< Reserved for Idle thread.
osPriorityLow = 8, ///< Priority: low
And also, the 'osThreadNew' does not let me create a task with priority '0', in 'cmsis_os2.c'
[...]
prio = (UBaseType_t)osPriorityNormal;
[...]
if (attr->priority != osPriorityNone) {
prio = (UBaseType_t)attr->priority;
}
if ((prio < osPriorityIdle) || (prio > osPriorityISR) || ((attr->attr_bits & osThreadJoinable) == osThreadJoinable)) {
return (NULL);
}
[...]
Is this a mistake? Or is the intended behaviour?
From my point of view:
The idle task is responsible for freeing memory allocated by the RTOS to tasks that have since been deleted.
It is therefore important in applications that make use of the vTaskDelete() function to ensure the idle task is not starved of processing time.
The idle task has no other active functions so can legitimately be starved of microcontroller time under all other conditions.
Looking forward for your answer,
Thanks,
Carles
Solved! Go to Solution.
2025-02-23 1:06 AM - edited 2025-02-23 1:32 AM
Your right if you want to use only the CMSIS V2 layer you cannot create a Task on the Idle priority..
You could use the Idle Hook, but this is also not CMSIS V2 compatible.
Or You could use the CMSIS V1 layer, I don't think that CMSIS V1 has the same limit.
P.S.: This seems to be corrected on the latest cmsis_v2.c from ARM (https://github.com/ARM-software/CMSIS-FreeRTOS/commit/9cdbe17d1b7704439a9e6a1fa50ef879eff9b913)
So ST should consider updating to a newer version of cmsis_v2.c
2025-02-21 10:36 AM
Cmsis_os2.c/h is wrapper to make FreeRTOS CMSIS compatible, so the priorities in cmsis_os2.h are different from the priorities used by FreeRTOS.
In FreeRTOS the Idle Thread is created automatically, you don't have to start or define it by yourself.
Martin
2025-02-22 9:43 AM
I understand it, thanks.
I already know that I don't need to create the Idle task by myself. My point is: if I want to work with FreeRTOS through CMSIS layer, I can not set another task with the same priority as the FreeRTOS Idle task, and that's a shame.
Thanks for your answer.
2025-02-23 1:06 AM - edited 2025-02-23 1:32 AM
Your right if you want to use only the CMSIS V2 layer you cannot create a Task on the Idle priority..
You could use the Idle Hook, but this is also not CMSIS V2 compatible.
Or You could use the CMSIS V1 layer, I don't think that CMSIS V1 has the same limit.
P.S.: This seems to be corrected on the latest cmsis_v2.c from ARM (https://github.com/ARM-software/CMSIS-FreeRTOS/commit/9cdbe17d1b7704439a9e6a1fa50ef879eff9b913)
So ST should consider updating to a newer version of cmsis_v2.c
2025-02-24 1:59 AM
Hello @MHoll.2 and @selracelosuarg
A request to update CMSIS V2 to the new version has been reported to the dev team.
Internal ticket number: 203833 (This is an internal tracking number and is not accessible or usable by customers).
2025-02-24 5:18 AM
Hello @selracelosuarg
Could you please specify which product you are using please?
2025-02-24 5:21 AM
Hi @Saket_Om ,
I am currently using as PoC the STM32H743 Nucleo-144 Board that comes with a 'STM32H743ZIT6 144 pins'.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.