2019-08-13 5:08 PM
Hi,
I'm trying to configure STM32H7 and STM32G4 FDCANs to generate an ISR on transmit complete frame.
I call the functios to enable respective ISRs:
HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_COMPLETE, 0);
HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_FIFO_EMPTY, 0);
When a FDCAN frame is trasmited, only TxFifoEmptyCallback notify an interrupt, there's no call to TxBufferCompleteCallback.
What am I missing?
2019-10-09 7:43 AM
It appears you are missing the last parameter in ActivateNotification:
* @param BufferIndexes Tx Buffer Indexes.
* This parameter can be any combination of @arg FDCAN_Tx_location.
* This parameter is ignored if ActiveITs does not include one of the following:
* - FDCAN_IT_TX_COMPLETE
* - FDCAN_IT_TX_ABORT_COMPLETE0 is not a valid option in the `FDCAN_Tx_location` group.
2020-02-25 12:15 AM
i'm having the same issue. if 0 isn't an acceptable third argument for (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_COMPLETE, 0), then what is? I can't find any information given on the task.
2020-02-25 6:38 AM
After Digging endlessly through the HAL code, I figured it out.
to activate TX IT complete notifications :
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_COMPLETE, FDCAN_TX_BUFFER0 | FDCAN_TX_BUFFER1 | FDCAN_TX_BUFFER2) != HAL_OK)
{
Error_Handler();
}
//then the interrupt function
// Transmission Complete callback FDCAN_Tx_location
void HAL_FDCAN_TxBufferCompleteCallback(FDCAN_HandleTypeDef *hfdcan, uint32_t BufferIndexes)
{
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_7);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.