STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to compare bytes received in a uint8_t?

I have a STM32F103C8T card, I am developing an application that receives a byte array by usb / serial.I have a variable "uint8_t USBBuffer;" in "usbd_cdc_if.c" which stores the bytes.My question is: how can a non-vector variable receive an external m...

Hi, I am using fatfs on flash along with usb msc device on stm32 mcu ,it is working usb detected I am able to do file operations and check files from desktop when plugged in the usb.

what i noticed is if i create n no of files, only 8 files are displayed however the remaining files are also created but not displayed, i am using elm chans fatfs. What could be the problem why only first 8 files displayed on pc .Kindly let me know ...

svii by Associate III
  • 1117 Views
  • 2 replies
  • 0 kudos

AN4826 Errors

There are a couple of inconsistencies in AN4826.First one that has been repeated in other posts is that there is a bug in the bootloader and BOOT0 pin's state is actually irrelevant as it always boots from BOOT_ADD0 anyway.So the select BOOT_ADDx bas...

Resolved! Controller stalls at NVIC_EnableIRQ(CAN_TX_IRQn) after jump to application from a bootloader.

Hi,I am using a CAN bootloader to update my application. But after flashing the application and jumping from the bootloader to the reset vector of the app, the program stalls after calling NVIC_EnableIRQ(CAN_TX_IRQn). Is there a problem that the boot...

0690X00000BufjIQAR.png 0690X00000BufjiQAB.png
MGand.1 by Associate II
  • 3178 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.