2020-09-03 12:09 AM
Hi
I've configured FatFs for SD 4Bit Bus. I'm using FreeRTOS.
When USE_LFN = 0 then all works well. Writing and reading to/from the SD card is working as it should.
As soon as I enable USE_LFN = 3 (in CubeMX) f_open returns FR_NO_FILESYSTEM (13).
check_fs in f_open return 2 (Valid BS but not FAT).
That's strange because I've formatted the SD card with f_mkfs as FAT and FAT32. I've formatted it on my PC as FAT and FAT32 as well. I always get this behaviour.
Can anyone help me with this issue?
Regards
Dejan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.