2021-10-08 10:56 PM
Hello,
i need your help where to start the project,
if i will get example for these type of application will also help me to start this,
Thanks
regards
< siva >
2021-10-08 11:12 PM
Does the F0 even have a USB Host Controller?
You could look in the CubeF0 board example trees for examples. MSC devices for sure.
2021-10-09 2:21 AM
2021-10-09 2:19 PM
HOST != DEVICE
For a DEVICE
STM32Cube_FW_F0_V1.10.1\Projects\STM32072B_EVAL\Applications\USB_Device\MSC_Standalone
2021-10-31 5:21 AM
Small Confusion between Host & Device,
Now its clear,
i selected the micro controller which is not work as a Host .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.