2022-02-14 1:58 AM
I have a STM32F429 Discovery board and I want to add ethernet for project. I am using external ethernet PHY named KSZ8863. Is it possible to
communicate with using this PHY ? if it is possible should you share an example code for it?
Solved! Go to Solution.
2022-02-14 12:22 PM
Welcome, @şükrü krc, to the community!
First of all, DISCOVERY boards are intended to investigate the functions of the respective STM32 and are therefore already equipped with plenty of peripherals so that you can test this extensively without having to build your own board. For this reason, only a few GPIOs are free for alternative use on the DISCOVERY boards. In your particular case, the pins you need for the interfaces MII or RMII are already occupied, so you cannot retrofit the STM32F429I-DISC1 with an Ethernet PHY via RMII/MII.
If you want not only to try out the functions of the respective STM32, but to have almost complete freedom in development, you should consider a NUCLEO board instead, e.g. the NUCLEO-F429ZI.
Good luck!
Regards
/Peter
2022-02-14 12:22 PM
Welcome, @şükrü krc, to the community!
First of all, DISCOVERY boards are intended to investigate the functions of the respective STM32 and are therefore already equipped with plenty of peripherals so that you can test this extensively without having to build your own board. For this reason, only a few GPIOs are free for alternative use on the DISCOVERY boards. In your particular case, the pins you need for the interfaces MII or RMII are already occupied, so you cannot retrofit the STM32F429I-DISC1 with an Ethernet PHY via RMII/MII.
If you want not only to try out the functions of the respective STM32, but to have almost complete freedom in development, you should consider a NUCLEO board instead, e.g. the NUCLEO-F429ZI.
Good luck!
Regards
/Peter
2022-02-20 10:37 PM
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.