2021-04-06 9:15 AM
TCP_ECHO_Server
When I open TCP port and send some data on that port. It works fine.
But if I open 2 tcp port at same IP and same port (Max port I can have 5) .So while receiving data on both i gets the data alternatively on each port.
I want data should travel on each port irrespective of the number. Because port is same.
2021-04-07 3:25 AM
Hello
>> I want data should travel on each port irrespective of the number. Because port is same.
I am not sure that lwip programmers took care about this special case to listen to two times the same port.
if packet is for x.x.x.x IP and y Port, what is the meaning to process the same packet 2 times?
Note that after processing an input buffer the processing callback frees the buffer so can't be processed second time.
2021-05-20 5:07 AM
Hi Vangelis
Sorry, I was not active for long time.
With respect to above issue, if packet is for x.x.x.x IP and y Port and let say packet is "abc".
I opened a tcp client on my laptop with x.x.x.x IP and y Port( Terminal-1). and i opened another terminal with same x.x.x.x IP and y Port.(called terminal-2)
Now when I send data "abc", I will receive"123" in return from my devices. So i receive "123" from my devices but it comes alternatively ( first on terminal-1 then on terminal 2).But it should come to both terminal simultaneously irrespective of the terminal.
Just like Wireshark software does.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.