2019-01-23 9:14 PM
Whereas selecting v1.3.0 downloads the full ~400Mb file. Anyone else having this problem ?
2019-01-24 12:14 AM
Hello,
Thanks for highlighting this issue. We are working to resolve this.
Kind Regards,
Imen
2019-01-25 12:10 AM
Hello @SWood.8 ,
This issue is fixed now and you can download the patch release v1.3.1.
Kind Regards,
Imen
2019-01-25 12:42 AM
Great : ) will do
2019-01-25 12:45 AM
It still doesn't show up in STM32CubeMX's "Check for Updates" list for me. Or maybe minor updates are not being listed there?
2019-02-12 1:32 AM
This is the situation today:
en.stm32cubeh7.zip --> v1.3.0 --> OK (394 MB)
en.stm32cubeh7_v_1-3-1 --> v1.3.1 --> CORRUPTED FILE - NOT OK! (4.93KB)
en.patch_cubeh7.zip --> v1.3.2 --> OK (1.14MB)
Question is: can we skip v1.3.1 and use directly 1.3.2?
Thanks
2019-02-12 2:59 AM
Hello,
You should use the new patch of STM32CubeH7 V1.3.2, which englobe new fix of UID_BASE definition to the CMSIS STM32H7xx include files and also the fix of LwIP and mbedTLS applications (added in the v1.3.1 patch)
The patch v1.3.1 will be removed from the ST web site.
Kind Regards,
Imen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.