2025-01-30 8:56 AM
I have spent over a week trying to get USB to work with my board, and have had no luck. As soon as the device detects the USB, the usb goes straight into a HOST_USER_UNRECOVERED_ERROR.
I have received almost no assistance from STM32 regarding this, even though I have made posts about it. Its like they give you 1 response then never reply. I am at a point where I'm not even expecting the help, but I just need to know if what I'm attempting to do is even possible, because I found out for some reason CMSIS_OS2 does not even work with the USB library.
2025-01-30 10:31 AM
> I am at a point where I'm not even expecting the help, but I just need to know if what I'm attempting to do is even possible
Yes, USB host works on the STM32F750. Here is one example:
2025-02-05 3:19 AM
Hi @Priyank
At this level, USB stack error message "HOST_USER_UNRECOVERED_ERROR " cannot explain the issue you are having! I suggest starting with basics. I recommend this MOOC - STM32 USB training - YouTube
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.