2019-08-01 2:48 PM
I'm developing an STM32F429-based high-speed USB audio device that uses a Microchip USB3320 external PHY and would benefit from a DFU mode.
Is there an example available anywhere for such a configuration?
The default bootloader present in system memory doesn't seem to support the external PHY, so a bootloader that does this would reside in flash memory, similar like this project here:
https://github.com/akospasztor/stm32-bootloader
Solved! Go to Solution.
2019-08-01 3:07 PM
Ah, that was obvious: there seems to be a option in CubeMX to create a DFU project. I will check that out, hope it will work with the HS PHY.
2019-08-01 3:07 PM
Ah, that was obvious: there seems to be a option in CubeMX to create a DFU project. I will check that out, hope it will work with the HS PHY.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.