2024-05-21 10:51 PM
Hi
I want to debug my Display ST7735 (128 x 128 px). For that i wrote a code which sets the screen line by line into green color. When i flash the code it works fine. When i try to debug nothing happens on the display.
What can i do that the display changes the color during debugging?
Here you see the configuration of the debugger:
Here you see a screenshot of the code where each pixel (x,y) is set to GREEN color with SPI. w and h are the width and height of the display in pixel.
This Code is from the adafruit library ST7735.
Thanks for your answer,
Raphael
2024-05-22 12:29 AM
Check signal timings with a scope or analyzer.
Review data sheet check if you can read back registers or WHOAMI register.
Check back light enabled. Fill frame buffer with different patterns.
2024-05-29 5:18 AM
Do you want to try testLines(uint16_t color)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.