2025-10-29 10:29 PM
Hello team,
Another day, new same issue. :pensive_face:
I have setup the DCMIPP PIPE 1 for the stm32n6570 DK, so that it dumps frames in address 0x34200000 which maps to SRAM3 begin address I have enabled bothe the memories SRAM3 and SRAM4 but with out software erase, I used the MX tool for project generation , I goal is to mimic the Continous Mode example provided by ST,
I have read about the appilication notes getting started with DCMIPP and the afew sections of intrest form the RM for the deve board on the topic.
I however face the challenge as stated in the Post Title, there Is are no interrups being called yet I set up the global intterrups for both the Pixel pipe and the CSI interfacing, "Still as shown in in the generated files" and set the clocks for the DCMIPP is set to 300Mhz and the CSI interface I had to manualy try setting up the input clock freq for the IMX335 module to 20Mz as the MX tool does not provide for its setting, but I have this code commented out as there was not change in the behavoir
I use the BSP bus pakage for the I2C communication, in outere to reduce the debug window,
My Question has any one knoledge about what could be going on wrongly, or what I have not done in order to have my setup running as expected, I have checked My project for any security blocks set up, by default, but none I have seen.
I noticed that the internal calls to the RCC may be ignored :crossed_fingers: as the IDE shows the intermost LL calls being greyed out. especially in the
#include "stm32n6xx_ll_bus.h" file
@FBL please help me out here.
Find most of your querries in the attached files,
2025-11-04 2:10 AM
Also, Is it mandatory to have security / DMA manually setup so as to be able to have dcmipp work correctly, cause I think my image data is being help in the dcmip periphral and not being written to memory hence being over written in the peripheral continouly, leading to the "
#define HAL_DCMIPP_ERROR_PIPE1_OVR (0x00000010U) /*!< Overrun error on pipe1 */
"
I am switching bwt sram3 frame address location [0x34200000] ,
and an SRAM2 global memory variable static uint8_t frame_buffer[50000] __attribute__((aligned(16)));
at different runs just to see if the issue arised from my choosen memory location.
I notice with the latter I can't view the memory content of sram3, in my project memory debug view but I can with the example project, but this should be solved by decimating the image and placing it in a smaller location with in sram2
pDecConfig.HRatio = DCMIPP_HDEC_1_OUT_4;
pDecConfig.VRatio = DCMIPP_VDEC_1_OUT_4;
if (HAL_DCMIPP_PIPE_SetDecimationConfig(&hdcmipp, DCMIPP_PIPE1, &pDecConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_DCMIPP_PIPE_EnableDecimation(&hdcmipp, DCMIPP_PIPE1) != HAL_OK)
{
Error_Handler();
}
This also fails.
The ISP main frame ID increaments however,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.