2025-04-03 9:42 PM - edited 2025-04-03 9:43 PM
Hello,
I am trying to realise my own bootloader on my STM32U575 and have found the following article:
https://community.st.com/t5/stm32cubeide-mcus/stm32u575-custom-bootloader-bootloader/td-p/584218
Unfortunately this does not work for me.
I am using a STM32u575VGT and the following code:
static void _bootJumpToFirmware() {
typedef void (*pFunction)(void);
#define APPLICATION_ADDRESS 0x0803C000
pFunction JumpToApplication;
JumpToApplication = (pFunction) (*(volatile uint32_t*) (APPLICATION_ADDRESS + 4));
__set_MSP(*(uint32_t*) APPLICATION_ADDRESS);
JumpToApplication();
}/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 768K
SRAM4 (xrw) : ORIGIN = 0x28000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 240K
}/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 768K
SRAM4 (xrw) : ORIGIN = 0x28000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x0803C000, LENGTH = 784K
}ICACH is disabled.
I have flashed the main project and the bootloader project and checked with the STM32CubeProgrammer that from 0x8000000 or from 0x0803C000 code is contained in the flash with the expected code length.
When I start the controller, I can see that the bootloader is running (with LEDs on my board) and at the point where it should jump to the firmware, the controller seems to stop or the firmware does not start.
What can I investigate to find the problem?
Solved! Go to Solution.
2025-04-07 12:53 AM
The following problems have arisen, which I have now been able to solve:
With these two steps, the function itself, the adaptation in the two linker files and the adaptation in system_stm32u5xx.c, the jump to the firmware now works.
@Tesla DeLorean thanks for the tip with the vector table.
2025-04-03 9:50 PM
Make sure the SystemInit code in each sets SCB->VTOR to the appropriate Vector Table address.
Would suggest you try stepping the transition code, making sure it enters your Reset_Handler
Have a UART working along with a HardFault_Handler that outputs actionable data.
2025-04-03 10:57 PM - edited 2025-04-03 10:59 PM
I have set
/************************* Miscellaneous Configuration ************************/
/*!< Uncomment the following line if you need to relocate your vector Table in
Internal SRAM. */
/* #define VECT_TAB_SRAM */
#define VECT_TAB_OFFSET 0x0003C000UL /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
/******************************************************************************/in system_stm32u6xx.c of the main project
With the SystemInit function below the SCB_->VTOR should be set
void SystemInit(void)
{
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 20U)|(3UL << 22U)); /* set CP10 and CP11 Full Access */
#endif
/* Reset the RCC clock configuration to the default reset state ------------*/
/* Set MSION bit */
RCC->CR = RCC_CR_MSISON;
/* Reset CFGR register */
RCC->CFGR1 = 0U;
RCC->CFGR2 = 0U;
RCC->CFGR3 = 0U;
/* Reset HSEON, CSSON , HSION, PLLxON bits */
RCC->CR &= ~(RCC_CR_HSEON | RCC_CR_CSSON | RCC_CR_PLL1ON | RCC_CR_PLL2ON | RCC_CR_PLL3ON);
/* Reset PLLCFGR register */
RCC->PLL1CFGR = 0U;
/* Reset HSEBYP bit */
RCC->CR &= ~(RCC_CR_HSEBYP);
/* Disable all interrupts */
RCC->CIER = 0U;
/* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
SCB->VTOR = SRAM1_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif
}If i call disassembly at the _bootJumpToFirmware function i get
515 static void _bootJumpToFirmware() {
_bootJumpToFirmware:
08002330: push {r7, lr}
08002332: sub sp, #8
08002334: add r7, sp, #0
522 JumpToApplication = (pFunction)(*((uint32_t *)((APPLICATION_ADDRESS) + 4U)));
08002336: ldr r3, [pc, #32] @ (0x8002358 <_bootJumpToFirmware+40>)
08002338: ldr r3, [r3, #0]
0800233a: str r3, [r7, #4]
523 __set_MSP(*(uint32_t*) APPLICATION_ADDRESS);
0800233c: ldr r3, [pc, #28] @ (0x800235c <_bootJumpToFirmware+44>)
0800233e: ldr r3, [r3, #0]
08002340: str r3, [r7, #0]
1155 __ASM volatile ("MSR msp, %0" : : "r" (topOfMainStack) : );
08002342: ldr r3, [r7, #0]
08002344: msr MSP, r3
1156 }
08002348: nop
524 JumpToApplication();
0800234a: ldr r3, [r7, #4]
0800234c: blx r3
525 }At 0800234c the R3 register contains 0x8059cd1
In the End the Code reaches the Infinite Loop in startup_stm32u575vgtx.s at 0x8002a20 with the call structure
- 0x805c970
- 0x805c804
- <signal handler called>() at 0xfffffb8
- WWDG_IRQHandler() at startup_stm32u575vgtx.s:115 0x8002a20
I have set a breakpoint in the reset_handler in startup_stm32u575vgtx.s of the bootloaderproject in line 62, but the breakpoint never triggers.
2025-04-07 12:53 AM
The following problems have arisen, which I have now been able to solve:
With these two steps, the function itself, the adaptation in the two linker files and the adaptation in system_stm32u5xx.c, the jump to the firmware now works.
@Tesla DeLorean thanks for the tip with the vector table.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.