2021-02-12 12:48 PM
Hi there,
I have an old joystick which i want to convert to a custom hid device, the stick has three shiftin registers (cd4201) which i am reading using spi1. I know these shift register are being read cause i am sending it to serialport3 (just for debugging)and read values in docklight.
I have set up mu nucleo F413ZH as a custom hid device and my computer is detecting it as hid game device. I have generated my own report descriptor and is 65 byte long.
Following some tutorials spread over the net i cant get it to work.
By not work i think my data is not being send by using the USBD_CUSTOM_HID_SendReport.
I have set my EPIN and EPOUT to 64 bytes as recommended in various topics. But nothing is happening . But when i set my EPIN to 2 bytes and EPOUT 64 byte buttons in my device manger flashing randomly. And Axis values are all over the place.
My code is not fully done jet, for now I just want to see if my buttons are working in my device manager.
I have added some code
Report descriptor
__ALIGN_BEGIN static uint8_t CUSTOM_HID_ReportDesc_FS[USBD_CUSTOM_HID_REPORT_DESC_SIZE] __ALIGN_END =
{
0x05, 0x01, // USAGE_PAGE (Generic Desktop)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x09, 0x04, // USAGE (Joystick)
0xa1, 0x01, // COLLECTION (Application)
0x05, 0x02, // USAGE_PAGE (Simulation Controls)
0x09, 0xbb, // USAGE (Throttle)
0x16, 0x01, 0x80, // LOGICAL_MINIMUM (-32767)
0x26, 0xff, 0x7f, // LOGICAL_MAXIMUM (32767)
0x75, 0x10, // REPORT_SIZE (16)
0x95, 0x01, // REPORT_COUNT (1)
0x81, 0x06, // INPUT (Data,Var,Rel)
0x05, 0x01, // USAGE_PAGE (Generic Desktop)
0x09, 0x30, // USAGE (X)
0x09, 0x31, // USAGE (Y)
0x09, 0x33, // USAGE (Rx)
0x09, 0x34, // USAGE (Ry)
0x16, 0x01, 0x80, // LOGICAL_MINIMUM (-32767)
0x26, 0xff, 0x7f, // LOGICAL_MAXIMUM (32767)
0x75, 0x10, // REPORT_SIZE (16)
0x95, 0x04, // REPORT_COUNT (4)
0x81, 0x02, // INPUT (Data,Var,Abs)
0x05, 0x01, // USAGE_PAGE (Generic Desktop)
0x05, 0x09, // USAGE_PAGE (Button)
0x19, 0x01, // USAGE_MINIMUM (Button 1)
0x29, 0x20, // USAGE_MAXIMUM (Button 32)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x01, // LOGICAL_MAXIMUM (1)
0x95, 0x20, // REPORT_COUNT (32)
0x75, 0x01, // REPORT_SIZE (1)
0x81, 0x02, // INPUT (Data,Var,Abs)
/* USER CODE BEGIN 0 */
//0x00,
/* USER CODE END 0 */
0xC0 /* END_COLLECTION */
};usbd_config.h
#define USBD_MAX_NUM_INTERFACES 1U
/*---------- -----------*/
#define USBD_MAX_NUM_CONFIGURATION 1U
/*---------- -----------*/
#define USBD_MAX_STR_DESC_SIZ 512U
/*---------- -----------*/
#define USBD_DEBUG_LEVEL 0U
/*---------- -----------*/
#define USBD_LPM_ENABLED 0U
/*---------- -----------*/
#define USBD_SELF_POWERED 1U
/*---------- -----------*/
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 65//byte
/*---------- -----------*/
#define USBD_CUSTOM_HID_REPORT_DESC_SIZE 65//byte
/*---------- -----------*/
#define CUSTOM_HID_FS_BINTERVAL 0x1U
/****************************************/
/* #define for FS and HS identification */
#define DEVICE_FS 0
#define DEVICE_HS 1USBD_customhid.h
#define CUSTOM_HID_EPIN_ADDR 0x81U
#define CUSTOM_HID_EPIN_SIZE 0x02U //0x02 original
#define CUSTOM_HID_EPOUT_ADDR 0x01U
#define CUSTOM_HID_EPOUT_SIZE 0x40U //0x02 original
#define USB_CUSTOM_HID_CONFIG_DESC_SIZ 41U
#define USB_CUSTOM_HID_DESC_SIZ 9U
#ifndef CUSTOM_HID_HS_BINTERVAL
#define CUSTOM_HID_HS_BINTERVAL 0x05U
#endif /* CUSTOM_HID_HS_BINTERVAL */
#ifndef CUSTOM_HID_FS_BINTERVAL
#define CUSTOM_HID_FS_BINTERVAL 0x01U
#endif /* CUSTOM_HID_FS_BINTERVAL */
#ifndef USBD_CUSTOMHID_OUTREPORT_BUF_SIZE
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 0x41U //byte
#endif /* USBD_CUSTOMHID_OUTREPORT_BUF_SIZE */
#ifndef USBD_CUSTOM_HID_REPORT_DESC_SIZE
#define USBD_CUSTOM_HID_REPORT_DESC_SIZE 0x41 //byte// original 163U
#endif /* USBD_CUSTOM_HID_REPORT_DESC_SIZE */
#define CUSTOM_HID_DESCRIPTOR_TYPE 0x21U
#define CUSTOM_HID_REPORT_DESC 0x22U
#define CUSTOM_HID_REQ_SET_PROTOCOL 0x0BU
#define CUSTOM_HID_REQ_GET_PROTOCOL 0x03U
#define CUSTOM_HID_REQ_SET_IDLE 0x0AU
#define CUSTOM_HID_REQ_GET_IDLE 0x02U
#define CUSTOM_HID_REQ_SET_REPORT 0x09U
#define CUSTOM_HID_REQ_GET_REPORT 0x01U
/**
* @}
*/Hope some can help out or point me in the right direction,
Thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.