2017-09-22 3:54 PM
I was using the I2C Configuration dialog today, and i messed things up, so i hit the Restore Default button at the bottom of the I2C peripheral properties dialog.
When i regenerated my project, it compiled with errors, because all my pin User Labels reset too!!!!
Even ones that had nothing to do with I2C, like buttons and LEDs, etc....
I am using v4.22.1. This is a bug!!!
The button on a peripheral config dialog should only reset the peripheral.
Its debatable if it should reset, the associated pins that have been given user labels.
It definitely should not reset other stuff, without a warning!
#cube #restore-default2018-02-06 6:15 AM
Hi
Craven.John
,Sorry for my late reply.
I see your point. We will keep you informed as soon as we have some updates on this topic.
BR. Jeanne
2018-02-07 6:50 AM
LOL! glad to see you are on it!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.