2016-02-19 12:47 AM
After compiling the CubeMX generated Code (without any changes).
The Ethernet stack crashes if it receives many UDP-packages in a short time. (1000-10000 10Byte packages in a few ms) Even after stopping the flood the interface never comes up again. The interface only comes back again if I call ''static void low_level_init(struct netif *netif)'' (without creating the thread and semaphore again) or after a software reset. This behaviour is really bad.Could you help me?
uC: STM32F437IITx
PHY: DP83848CubeMX 4.13.0 (Firmware Package for Family STM32F4 1.11.0):
- FREERTOS - [x] Enabled - LWIP - [x] Enabled - ETH: - Mode: MII - [ ] Activate Rx Err signal - RCC: - High Speed Clock (HSE): Crystal/Ceramic Resonator - Low Speed Clock (LSE): Disable - [x] Master Clock Output 1 - [ ] Master Clock Output 2 - [ ] Audio Clock Input (I2S_CKIN) - SYS: - Debug: JTAG (5 pins) - [ ] System Wake-Up - Timebase Source: TIM6 ETH_COL is sticked to pin PA3.LWIP settings:
- IP_ADDRESS (IP Address): 192.168.001.049 - NETMASK_ADDRESS (Netmask Address): 255.255.255.000Another error, which has nothing to do with the upper one, is (stm32f4xx_hal_conf.h):
&sharpdefine PHY_MICR_INT_OE ((uint16_t)0x0002U) /*!< PHY Enable output interrupt events */It should be:
&sharpdefine PHY_MICR_INT_OE ((uint16_t)0x0001U) /*!< PHY Enable output interrupt events */ #freertos #lwip #stm32f42016-02-24 5:52 AM
Hi di.lau,
The issues are reported internally to be checked by CubeMX team.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-03-03 6:18 AM
Do you have some new information?
2016-05-11 2:37 AM
Dear user,
Please upgrade to next version 4.15 (available soon) that will fix these issues. Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.