2017-04-13 5:09 AM
Hello I use project CDC Virtual COM Port, which I few change. My project has 2 endpoints. Bulk - out and Interrupt - in. I use standart function: CDC_Receive_HS (uint8_t* Buf, uint32_t *Len) - for receive data and CDC_Transmit_HS(uint8_t* Buf, uint16_t Len) - for transmit data. When I
periodically
call CDC_Transmit_HS in main program, I sometimes can't receive data from Bulk. Why ?When I call CDC_Transmit_HS in USB SOF interrupt, I
always receive data from Bulk and It work good.
#cubef4 #interrupt #usb #bulkWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.