STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32l1xx_ll_spi.h BUG and Warning

Posted on December 15, 2016 at 18:16Dear SirsFile : stm32l1xx_ll_spi.hVery ugly BUG !!!!__STATIC_INLINE void LL_GPIO_ResetOutputPin(GPIO_TypeDef *GPIOx, uint32_t PinMask){!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!...

How to disable USB interrupt if it's not needed ?

Posted on March 12, 2017 at 00:40Everyone,I have a question :How to disable USB interrupt if it's not needed ? I used USB as MSD and it's using SDIO, any method to handle it ? And SDIO is working together with SPI.So far I'm playing with usbd_storag...

HAl_uart recive interrupt

Posted on March 11, 2017 at 08:55I am facing problem that i am trying to receive data on uart_2 but the interrupt get disable automatically  after some transitions i have check the RXNEIE register. Can any one guide to me the problem and its solutio...

daynial by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos

HAL De-Init Pin for use with another peripheral

Posted on March 09, 2017 at 08:11Good DayI am using the built-in comparator on a STM32F072RB. The comparator works fine, but now I want to be able to measure the amplitude of the sine-wave (already withing 0-3.3V limits) by 'removing' the pin from t...

abotha by Associate III
  • 897 Views
  • 1 replies
  • 0 kudos

STM32 L4 ADC accuracy

Posted on March 07, 2017 at 14:32Hello,I'm working with the STM32L475 micro. In my application I read several analog values using the ADC1. Values read are quite similar when device is in run mode. But, according to my specs and in order to save pow...

Is it possible to measure TTL signal levels at stm32L4 CAN pin Tx without being integrated into a can net?

Posted on March 08, 2017 at 14:25I'm using HAL_CAN_transmit to send data for stm32L4 mcu. I'm trying to send frames with 2 bytes in an infinite loop.I would like to know if it's possible and if feasible to measure TTL signal levels at GPIO TX pin of...

General Documentation for Ethernet PHY registers

Posted on March 07, 2017 at 17:54I am working on a board (STM32F407VGTx) that has an older PHY chip KSZ8721BL. I have similar code running on the MCBSTM32F400 (v1.2) which has an KSZ8081RNA. In testing, I retrieved all of the registers from both PHY...

dibs by Associate II
  • 1460 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.