2022-04-12 5:54 AM
In the OTG USB implementation, in USB_DevInit(), the PFIVL field of OTG_FS_DCFG is supposed to be written, eg. here, in the following way:
USBx_DEVICE->DCFG |= DCFG_FRAME_INTERVAL_80;
the DCFG_FRAME_INTERVAL_xx constants are defined in the respective header as 0, 1, 2, 3; i.e. the value of the bitfield. It means, that before ORing, they need to be left-shifted by USB_OTG_DCFG_PFIVL_Pos, which is nonzero.
Now the exact constant DCFG_FRAME_INTERVAL_80 is zero, and the default value of PFIVL field is zero too, so as it is now it is entirely harmles; a bug nonetheless.
Checked in CubeL4 and CubeF4 as of now (12.Apr 2022) it was the same; probably it's same in all OTG implementations.
JW
2022-04-14 3:43 AM
Hello @Community member ,
Thank you for your feedback.
I escalated this issue internally to the appropriate team (Internal ticket number 126442).
I will get back to you soon with update.
Thanks
Imen
2022-04-14 2:31 PM
Thanks Imen.
There's no need to pay more attention to this, it's a minor and in its present state harmless issue. Just trying to improve.
Jan
2023-06-12 9:14 AM
Looks like this did not stick.
JW
@Imen DAHMEN
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.