STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M4 core heap issue on STM32H745.

I am working on STM32H745 discovery board. I have the following peripherals configured on both cores-Cortex M4- FreertosCortex M7- Freertos, Ethernet, LWIP, USART, QSPI, SDRAM.In M4 core there is a default task in which LED is blinking. When I enable...

Akast.2 by Associate II
  • 1628 Views
  • 1 replies
  • 0 kudos

Error in 'en.stsw-stm32156' - AN4457 ?

Hello,can someone confirm that line 890 /* Disable External interrupt for next Frame */ EXTI->IMR &= ~EXTI_EMR_MR3;is not correct in 'stm32f4xx_hal_uart_emul.c'?Everywhere else it is written something like this EXTI->IMR |= huart_emul->Init....

SMauch by Associate
  • 1397 Views
  • 1 replies
  • 0 kudos

How to do authorization on STM32 and LWIP?

I want to implement authorization on STM32 and LWIP.I took this examplehttps://github.com/particle-iot/lwip-contrib/blob/master/examples/httpd/post_example/post_example.cbut it doesn't work. Session.html is available without authorizationWhat could b...

DK.7 by Senior
  • 2206 Views
  • 2 replies
  • 0 kudos

Resolved! New Lib reentrant using C++ and RTOS

I am confused on the topic of new lib reentrant and RTOS.I use C++ and do some std::make_unique calls so malloc it's probably getting called under the hood.I have enabled the setting configUSE_NEWLIB_REENTRANT for RTOS and I am using heap_4 memory sc...

MC.5 by Associate II
  • 5205 Views
  • 4 replies
  • 1 kudos

Resolved! Hard fault, vector table | jump from boot to app

I'm using Keil (Scatter file, not lnker) and I have a bootloader and a place for two images (one active and other is for the over the air update).i use Cortex M0 processor where there is no Vector Table Offset Register and i used to copy the vector t...

Vmere.1 by Senior
  • 6682 Views
  • 10 replies
  • 0 kudos

Failed to execute .localhost:61234

Hi, i have recently purchased an STM32F746G-DISCO.i am very new to STM and compontents, but my manager would like me to try and build an interest with it. I followed a tutorial online, and i have followed the exact routes but i keep getting this erro...

JLythgoe by Associate
  • 2748 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.