2026-02-13 5:17 AM - last edited on 2026-02-18 3:40 AM by mƎALLEm
To follow up this thread, CTS signal on USB CDC - STMicroelectronics Community
I'm experiencing a similar issue.
USBser.sys have some problem
1. Only DTR Break can control alone
you can set DTR is 1 or 0, but RTS have change,RTS only change with DTR.
2. CDC Serial State
I have test this code, it send from Endpoint 81h successfully, but PC USB Host have no message
CDC_IN_Buf[0] = 0xA1; /* bmRequestType 0xA1 (10100001B) */
CDC_IN_Buf[1] = 0x20; /* 0x21 (SERIAL_STATE) */
CDC_IN_Buf[2] = 0x00; /* wValue LowByte */
CDC_IN_Buf[3] = 0x00; /* wValue HiByte */
CDC_IN_Buf[4] = 0x00; /* wIndex LowByte Default 0 */
CDC_IN_Buf[5] = 0x00; /* wIndex HiByte */
CDC_IN_Buf[6] = 0x02; /* wLength LowByte Serial State Length 0x0002 */
CDC_IN_Buf[7] = 0x00; /* wLength HiByte */
CDC_IN_Buf[8] = 0x14; /* Data LowByte */
CDC_IN_Buf[9] = 0x00; /* Data HiByte */
/*
CDC Serial State bit define (USB CDC 1.1 6.3.5 )
bit0 bRxCarrier 0x01
bit1 bTxCarrier 0x02
bit2 bBreak 0x04
bit3 bRingSignal 0x08
bit4 bFraming 0x10
bit5 bParity 0x20
bit6 bOverRun 0x40
*/
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, CDC_IN_Buf, 10);
USBD_LL_Transmit(&hUsbDeviceFS, CDC_CMD_EP, CDC_IN_Buf, 10);Solved! Go to Solution.
2026-03-01 9:04 PM
/**
* @brief USBD_CDC_Setup
* Handle the CDC specific requests
* @PAram pdev: instance
* @PAram req: usb requests
* @retval status
*/
static uint8_t USBD_CDC_Setup(USBD_HandleTypeDef *pdev,
USBD_SetupReqTypedef *req)
{
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassDataCmsit[pdev->classId];
uint16_t len;
uint8_t ifalt = 0U;
uint16_t status_info = 0U;
USBD_StatusTypeDef ret = USBD_OK;
if (hcdc == NULL)
{
return (uint8_t)USBD_FAIL;
}
switch (req->bmRequest & USB_REQ_TYPE_MASK)
{
case USB_REQ_TYPE_VENDOR: /* 0x40 Request from vendor */
#if defined(USE_CH340_DRIVER)
CH340_Requset_Handle(pdev, hcdc, req);
#elif defined(USE_FTDI_DRIVER)
FT232RL_Requset_Handle(pdev, hcdc, req);
#endif
break;
case USB_REQ_TYPE_CLASS: /* 0x20 CDC HID UVC UAC BOT Request */
...
2026-03-01 9:11 PM
1. RTS / DTR is use Control the other STM32 MCU Boot0/Reset pin.
2. Serial Status Notify is use PC Software the USB Device is wake or Data Package is read for transfer.
None of these ST have been implemented
2026-03-01 9:22 PM
RTS is not used for flow control. RTS is used to control the Boot0 of a third-party STM32 MCU.
DTR is used to control the RESET of a third-party STM32 MCU.
Serial port status notifications are used to inform the PC software that it is ready to receive packet data transmission from the USB CDC device, which is at a lower level than protocols like YModem.
2026-03-01 9:27 PM
RTS is not used for flow control. RTS is used to control the Boot0 of a third-party STM32 MCU.
DTR is used to control the RESET of a third-party STM32 MCU.
Serial port status notifications are used to inform the PC software that it is ready to receive packet data transmission from the USB CDC device, which is at a lower level than protocols like YModem.
Currently using the CH340 driver, the RTS control issue and the problem of reporting serial port status notifications to the PC host have been resolved. ST's driver is helpless with these two issues.
2026-03-02 7:34 AM
Thank you @wjandsq for explanation of your use case. Hope someone from ST can follow up.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.