2018-05-16 7:07 PM
Dear All;
I would like to know when I have array and I would like to convert array to string.
char A[6] = { 'A', 'B', 'C', 'D', 'E', 'F', 'G' };
char *B;
I would like to
*B = 'ABCDEFG';
How should I do?
#c #hal2018-05-16 7:32 PM
Hi
When you have a string such as 'ABCDEFG' it actually takes 8 characters and is found in memory as:
'A'
'B'
'C'
'D'
'E'
'F'
'G'
'\0'
So you should get a compiler error in your code since you only declared 6 elements of the array but actually have 7 in the assignments. But assuming you correct that, you still need to allocate an 8th character as '\0' as the string terminator.
Once that is corrected a pointer to char can be re-cast to point to an array of chars so you could say:
B = A;
As a homework assignment, what would happen if you did not declare the 8th character as '\0'? Would you get an error with your statement B=A? Answer back.
Regards
Bill2018-05-16 7:45 PM
Dear Bill;
Thank you for your answer. I would like to know how I convert array to string. I would like to compare string when I received UART message.
I received
char A[8] = { 'A', 'B', 'C', 'D', 'E', 'F', 'G' };
and I would like to compare to function 'if'. How should I do?
Such as :
if(A[8] == '9600')
{
foo();
}
else
{
while(1);
}
Regards
Mr.G
2018-05-16 8:53 PM
char *B;
B = 'ABCDEFG';
For compare see strcmp(), strncmp() or memcmp()
2018-06-07 3:01 AM
Thank you. I am done.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.