2020-04-25 9:56 AM
Hi guys,
i just wanted to mention that there is a ****** in the header files.
I am using an STM32G474:
Just an example - stm32g474xx.h defines
#define COMP3 ((COMP_TypeDef *) COMP3_BASE)And core_cm4.h uses
__IOM uint32_t COMP3; /*!< Offset: 0x050 (R/W) Comparator Register 3 */as part of DWT_Type.
Same applies to COMP2 and so on.
Good luck fixing this. Basically you have to rename the comparators.
2020-05-04 5:33 AM
Hi @Albi G. ,
Thanks for raising this issue. It is reported internally.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.