2021-11-17 9:35 PM
Can we mount the two devices i.e sd card and usb at a same time using FATFS in STM32F429ZI. I want to store the sensor data in SD card and copy that data to USB drive when the usb is detected. I am able to mount one device at a time. i have used user define fatfs for SD card and USB disk FatFs for USB. When i used both mode at a time the SD card is not able to mount. when i disable the USB mode in fatfs SD card is mounting as expected but not able to mount two devices at a time.
void sd_card_write()
{
// f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(buffer));
fresult = f_mount(&sd_fs, "0:", 1);
if (fresult != FR_OK)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, 0);
}
else
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 0);
}
/**************** The following operation is using f_write and f_read **************************/
/* Create second file with read write access and open it */
fresult = f_open(&sd_file, "0:FILE.TXT", FA_OPEN_EXISTING | FA_WRITE | FA_OPEN_APPEND);
/* Writing text */
sprintf(buffer,"Temperature:%f\n",Temp);
fresult = f_write(&sd_file, (const void *)buffer, strlen(buffer), &bw);
/* Close file */
f_close(&sd_file);
clear_buffer();
//unmount sd card
f_mount(&sd_fs, "0:", 0);
}
switch(Appli_state)
{
case APPLICATION_IDLE:
break;
case APPLICATION_START:
if(f_mount(&usb_fs, "1:", 0) == FR_OK)
{
//(TCHAR const*)USBH_Path
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_11, 1);
}
break;
case APPLICATION_READY:
{
UsbTest_Write();
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, 1);
HAL_Delay(5);
}
break;
case APPLICATION_DISCONNECT:
//unmount usb
f_mount(&usb_fs, "1:", 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_11, 0);
break;
}
bool UsbTest_Write(void)
{
//Open or Create file for writing
/* f_open(&sd_file, "FILE.TXT", FA_READ);
f_open(&usb_file, "Demo.TXT", FA_OPEN_EXISTING | FA_WRITE);
for (;;) {
fresult = f_read(&sd_file, buffer, sizeof(buffer), &br);
if (br == 0) break;
fresult = f_write(&usb_file, buffer, br, &bw);
if (bw < br) break;
}
f_close(&usb_file);
return 1; //Success
*/
if(f_open(&usb_file, "1:File.TXT", FA_OPEN_EXISTING | FA_WRITE | FA_OPEN_APPEND) != FR_OK)
{
return 0;
}
//Copy test Text to my temporary read/write buffer
sprintf(rwtext, "Temp:%f\n",Temp);
//Write to text file
fresult = f_write(&usb_file, (const void *)rwtext, strlen(rwtext), &bw);
if((fresult != FR_OK) || (bw == 0))
{
return 0;
}
f_close(&usb_file);
return 1; //Success
}
//2. USB test Read function
bool UsbTest_Read(void)
{
//Open file for reading
if(f_open(&usb_file, "1:File.TXT", FA_READ) != FR_OK)
{
return 0;
}
//Read text from files until NULL
for(uint8_t i=0; i<100; i++)
{
fresult = f_read(&usb_file, (uint8_t*)&rwtext[i], 1, &br);
if(rwtext[i] == 0x00) // NULL string
{
br = i;
break;
}
}
//Reading error handling
if(br==0) return 0;
//Close file
f_close(&usb_file);
return 1; // success
}
2021-11-17 10:01 PM
Hi @Nikhil Gayke
yes you can, have a look at this project it links the SD & SDRAM drives using FatFs, you can do the same using the USB & SD.
the main trick is to define "_VOLUMES = 2" in the ffconf.h
regards
Haithem.
2021-11-17 10:08 PM
yes i have define _VOLUMES = 2 still its not working. How to link the USB and SD drive Using FatFs
2021-11-17 10:12 PM
This is the code
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "fatfs.h"
#include "usb_host.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "fatfs_sd.h"
#include "string.h"
#include "stdio.h"
#include <stdbool.h>
ADC_HandleTypeDef hadc3;
SPI_HandleTypeDef hspi1;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
static void MX_ADC3_Init(void);
void MX_USB_HOST_Process(void);
/* USER CODE BEGIN PFP */
//1. USB test Write function
bool UsbTest_Write(void);
//2. USB test Read function
bool UsbTest_Read(void);
/* USER CODE END PFP */
extern ApplicationTypeDef Appli_state;
//USB Logical path
char USBH_Path[4]; /* USBH logical drive path */
char rwtext[100];
FATFS sd_fs,usb_fs; // file system
FIL sd_file,usb_file; // File
FILINFO fno;
FRESULT fresult; // result
UINT br, bw; // File read/write count
float adc_val=0;
float Temp;
float resolution;
#define BUFFER_SIZE 100
char buffer[BUFFER_SIZE]; // to store strings..
int i=0;
int bufsize (char *buf)
{
int i=0;
while (*buf++ != '\0') i++;
return i;
}
void clear_buffer (void)
{
for (int i=0; i<BUFFER_SIZE; i++) buffer[i] = '\0';
}
void adc_value()
{
HAL_ADC_Start(&hadc3);
HAL_ADC_PollForConversion(&hadc3, 10);
adc_val=HAL_ADC_GetValue(&hadc3);
resolution=( 3.0/4095.0);
Temp=(adc_val * resolution * 100);
HAL_Delay(10);
}
void sd_card_write()
{
fresult = f_mount(&sd_fs, "0:", 1);
if (fresult != FR_OK)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, 0);
}
else
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 0);
}
/* Create second file with read write access and open it */
fresult = f_open(&sd_file, "0:FILE.TXT", FA_OPEN_EXISTING | FA_WRITE | FA_OPEN_APPEND);
/* Writing text */
sprintf(buffer,"Temperature:%f\n",Temp);
fresult = f_write(&sd_file, (const void *)buffer, strlen(buffer), &bw);
/* Close file */
f_close(&sd_file);
clear_buffer();
//unmount sd card
f_mount(&sd_fs, "0:", 0);
}
int main(void)
{
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_SPI1_Init();
MX_FATFS_Init();
MX_ADC3_Init();
MX_USB_HOST_Init();
/* USER CODE BEGIN 2 */
HAL_ADC_Start(&hadc3);
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
adc_value();
sd_card_write();
switch(Appli_state)
{
case APPLICATION_IDLE:
break;
case APPLICATION_START:
if(f_mount(&usb_fs, "1:", 0) == FR_OK)
{
//(TCHAR const*)USBH_Path
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_11, 1);
}
break;
case APPLICATION_READY:
{
UsbTest_Write();
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, 1);
HAL_Delay(5);
}
break;
case APPLICATION_DISCONNECT:
//unmount usb
f_mount(&usb_fs, "1:", 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_11, 0);
break;
}
}
/* USER CODE END 3 */
}
void SystemClock_Config(void)
{
}
static void MX_ADC3_Init(void)
{
}
static void MX_SPI1_Init(void)
{
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
}
//1. USB test Write function
bool UsbTest_Write(void)
{
//Open or Create file for writing
/* f_open(&sd_file, "FILE.TXT", FA_READ);
f_open(&usb_file, "Demo.TXT", FA_OPEN_EXISTING | FA_WRITE);
for (;;) {
fresult = f_read(&sd_file, buffer, sizeof(buffer), &br);
if (br == 0) break;
fresult = f_write(&usb_file, buffer, br, &bw);
if (bw < br) break;
}
f_close(&usb_file);
return 1; //Success
*/
if(f_open(&usb_file, "1:File.TXT", FA_OPEN_EXISTING | FA_WRITE | FA_OPEN_APPEND) != FR_OK)
{
return 0;
}
//Copy test Text to my temporary read/write buffer
sprintf(rwtext, "Temp:%f\n",Temp);
//Write to text file
fresult = f_write(&usb_file, (const void *)rwtext, strlen(rwtext), &bw);
if((fresult != FR_OK) || (bw == 0))
{
return 0;
}
f_close(&usb_file);
return 1; //Success
}
//2. USB test Read function
bool UsbTest_Read(void)
{
//Open file for reading
if(f_open(&usb_file, "1:File.TXT", FA_READ) != FR_OK)
{
return 0;
}
//Read text from files until NULL
for(uint8_t i=0; i<100; i++)
{
fresult = f_read(&usb_file, (uint8_t*)&rwtext[i], 1, &br);
if(rwtext[i] == 0x00) // NULL string
{
br = i;
break;
}
}
//Reading error handling
if(br==0) return 0;
//Close file
f_close(&usb_file);
return 1; // success
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2021-11-17 10:16 PM
char RAMpath[4], SDpath[4]; /* RAM disk and SD card logical drives paths */
if((FATFS_LinkDriver(&SDRAMDISK_Driver, RAMpath) == 0) && (FATFS_LinkDriver(&SD_Driver, SDpath) == 0))
{
/*##-2- Register the file system object to the FatFs module ##############*/
res1 = f_mount(&RAMFatFs, (TCHAR const*)RAMpath, 0);
res2 = f_mount(&SDFatFs, (TCHAR const*)SDpath, 0);
if((res1 != FR_OK) || (res2 != FR_OK))
{
/* FatFs Initialization Error */
Error_Handler();
}Above how the RAM & SD are linked you'll need to replace the SRAM with USB drive, below the code snippet extracted from FatFs_USBDisk_RTOS
/* Link the USB Host disk I/O driver */
if(FATFS_LinkDriver(&USBH_Driver, USBDISKPath) == 0)
{
/* Init Host Library */
USBH_Init(&hUSBHost, USBH_UserProcess, 0);
/* Add Supported Class */
USBH_RegisterClass(&hUSBHost, USBH_MSC_CLASS);
/* Start Host Process */
USBH_Start(&hUSBHost);
2021-11-19 1:57 AM
I think in new version or cubemx by default link the driver at the time of initialization
void MX_FATFS_Init(void)
{
retUSBH = FATFS_LinkDriver(&USBH_Driver, USBHPath);
retUSER = FATFS_LinkDriver(&USER_Driver, USERPath);
}
but i tried to linked it again but its not working i am using STM32F429ZIT6U board does the board support the mounting of SD card and USB at a time because the there is difference in mounting of SD card & RAM and SD card & USB.
The main problem is both the devices get detected or get mounted when i use f_mount but the file that is get be stored in SD card is will be get stored in USB and SD card not have any file
void sd_card_write()
{
FATFS_LinkDriver(&USER_Driver, USERPath);
fresult = f_mount(&sd_fs, (TCHAR const*)USERPath, 1);
if (fresult != FR_OK)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, 0);
}
else
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, 1);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 0);
}
fresult = f_open(&sd_file, "0:FILE.TXT", FA_OPEN_EXISTING | FA_WRITE| FA_WRITE | FA_OPEN_APPEND);
sprintf(buffer,"Temperature:%f\n",Temp);
fresult = f_write(&sd_file, (const void *)buffer, strlen(buffer), &bw);
f_close(&sd_file);
clear_buffer();
FATFS_UnLinkDriver(USERPath);
}
void UsbTest_Write(void)
{
f_open(&sd_file, "0:FILE.TXT", FA_READ);
f_open(&usb_file, "1:FILE1.TXT", FA_OPEN_EXISTING |FA_WRITE | FA_OPEN_APPEND);
f_lseek(&sd_file, 0);
f_read(&sd_file, (void *)buffer1, strlen(buffer1), (void *)&bw1 );
f_write(&usb_file, buffer1, strlen(buffer1), (void *)&bw1);
f_close(&sd_file);
f_close(&usb_file);
}
switch(Appli_state)
{
case APPLICATION_IDLE:
break;
case APPLICATION_START:
FATFS_LinkDriver(&USBH_Driver, USBHPath);
if(f_mount(&usb_fs, (TCHAR const*)USBHPath, 0) == FR_OK)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_11, 1);
}
break;
case APPLICATION_READY:
{
UsbTest_Write();
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_12, 1);
HAL_Delay(5);
}
break;
case APPLICATION_DISCONNECT:
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_11, 0);
FATFS_UnLinkDriver(USBHPath);
break;
}
2021-11-19 4:57 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.