2024-11-26 7:17 AM
I need to have USB PD connectivity so I am using the examples provided. There are SNK and SRC and DRP examples. However, they all use the TCPP which is also included in all of the 3 demo boards. I don't see any way to disable the TCPP component itself and keep using the X-CUBE-TCPP middleware because it seems there is a library file provided that has the TCPP manipulation within it and I can't edit that file.
Is there any recommended strategy for developing a USBPD application on the STM32G071 that does not include the use of the TCPP hardware? I can uncheck the Board Part and the Board Support package but then I don't get good code generation.
Thanks
Solved! Go to Solution.
2024-12-03 6:34 AM
Hi @Carl_G
Sure, USB PD can be used without the TCPP hardware.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-03 6:34 AM
Hi @Carl_G
Sure, USB PD can be used without the TCPP hardware.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.