2025-07-07 2:19 AM
Hi, I have a problem with pinging PCs with my adapter USB-Ethernet with an STM32F207. I'm currently working with CDC-ECM for Ethernet-Over-USB.
First case: I have 2 VMs with Linux on them. The USB is connected to the first VM (VM1) and the Ethernet is connected to the second (VM2). I can ping VM1 with VM2 but I can't ping VM2 with VM1.
Second case: I have one VM with Linux and a Windows machine. The USB is connected to the VM and the ethernet is connected to the Windows machine. When I ping the VM with Windows or Windows with the VM I have only loss packets...
Does someone have any idea why ?
Thanks,
Solved! Go to Solution.
2025-07-08 11:50 PM
Hello @STackPointer64 ,
Thanks for your help :)
The problem was the checksum of the STM32.
Solution :
In my code I change CHECKSUM_BY_HARDWARE to CHECKSUM_BY_SOFTWARE. And everything works fine.
2025-07-07 3:43 AM - edited 2025-07-07 3:44 AM
Hello @Gwen1,
Case 1: Two Linux VMs
ip addr,ip route and in your virtualization application settings. Make sure they are in the same subnet or have proper routing rules.ip link show), with the correct IP assigned.sudo iptables -F and sudo ufw disable) to rule out any ICMP blocking.arp -n) to ensure MAC address resolution is working; if ARP fails, packets won’t be delivered.dmesg) for any errors or dropped packets.Case 2: Linux VM and Windows machine
ipconfig /all on Windows; ip addr and ip route on Linux).netsh advfirewall firewall add rule name="ICMP Allow inbound" protocol=icmpv4:8,any dir=in action=allow
dmesg for any driver errors.ethtool on Linux if available.arp -a on Windows, arp -n on Linux), since failure here will cause ping to fail.Best regards,
2025-07-08 11:50 PM
Hello @STackPointer64 ,
Thanks for your help :)
The problem was the checksum of the STM32.
Solution :
In my code I change CHECKSUM_BY_HARDWARE to CHECKSUM_BY_SOFTWARE. And everything works fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.