2020-10-23 10:43 AM
I am trying to setup USB communication with an STM32F446RE
It is a custom board where:
The external quartz is working (I can load a firmware that just blinks a led) but I fail to enumerate the USB device with below message in the computer syslog.
I am using mbed with the NUCLEO F446RE configuration, I just enabled USB in the target configuration (USE_USB_OTG_FS type)
Also, I noted that if I plug the board even without a firmware that is supposed to use USB, my computer tries to enumerate the device, however it shows a different message (like it's trying to enumerate a low-speed device instead of high-speed)
Do you have any idea/clue what could be going wrong?
Oct 23 19:13:51 destiny kernel: [4213209.733361] usb 1-10: new full-speed USB device number 17 using xhci_hcd
Oct 23 19:13:51 destiny kernel: [4213209.861500] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:51 destiny kernel: [4213210.097415] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:51 destiny kernel: [4213210.333311] usb 1-10: new full-speed USB device number 18 using xhci_hcd
Oct 23 19:13:51 destiny kernel: [4213210.461545] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:52 destiny kernel: [4213210.697528] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:52 destiny kernel: [4213210.805438] usb usb1-port10: attempt power cycle
Oct 23 19:13:52 destiny kernel: [4213211.461355] usb 1-10: new full-speed USB device number 19 using xhci_hcd
Oct 23 19:13:52 destiny kernel: [4213211.461721] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213211.669583] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213211.877357] usb 1-10: device not accepting address 19, error -71
Oct 23 19:13:53 destiny kernel: [4213212.005324] usb 1-10: new full-speed USB device number 20 using xhci_hcd
Oct 23 19:13:53 destiny kernel: [4213212.005568] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213212.213745] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213212.421346] usb 1-10: device not accepting address 20, error -71
Oct 23 19:13:53 destiny kernel: [4213212.421442] usb usb1-port10: unable to enumerate USB device
Solved! Go to Solution.
2020-10-23 2:20 PM
Pull BOOT0 High, and see if your hardware populates as a USB STM32 DFU device.
Check what you HSE does, output via MCO, check speed to come up.
Make sure PLL comes up, make sure PLL is generating 48 MHz for USB
Check D+/D- not backward
2020-10-23 12:55 PM
IMO Nucleo does not have a crystal this used HSE in Bypass more.
Otherwise, debug as usually, it is your code now.
JW
2020-10-23 2:19 PM
Ok actually it was a really stupid problem, I shorted VUSB and D- when soldering the micro USB port :grinning_face_with_sweat:
2020-10-23 2:20 PM
Pull BOOT0 High, and see if your hardware populates as a USB STM32 DFU device.
Check what you HSE does, output via MCO, check speed to come up.
Make sure PLL comes up, make sure PLL is generating 48 MHz for USB
Check D+/D- not backward
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.