cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: v1.8.0 stm32h7xx_hal_spi in IRQHandler

JLata
Associate

There is a bug in the IRQHandler function that causes the callbacks associated not being correctly called.

      hspi->State = HAL_SPI_STATE_READY; 
      if (hspi->ErrorCode != HAL_SPI_ERROR_NONE)
      {
#if (USE_HAL_SPI_REGISTER_CALLBACKS == 1UL)
        hspi->ErrorCallback(hspi);
#else
        HAL_SPI_ErrorCallback(hspi);
#endif /* USE_HAL_SPI_REGISTER_CALLBACKS */
        return;
      }
    }
 
#if (USE_HAL_SPI_REGISTER_CALLBACKS == 1UL)
    /* Call appropriate user callback */
    if (State == HAL_SPI_STATE_BUSY_TX_RX)
    {
      hspi->TxRxCpltCallback(hspi);
    }
    else if (State == HAL_SPI_STATE_BUSY_RX)
    {
      hspi->RxCpltCallback(hspi);
    }
    else if (State == HAL_SPI_STATE_BUSY_TX)
    {
      hspi->TxCpltCallback(hspi);
    }
#else
    /* Call appropriate user callback */
    if (State == HAL_SPI_STATE_BUSY_TX_RX)
    {
      HAL_SPI_TxRxCpltCallback(hspi);
    }
    else if (State == HAL_SPI_STATE_BUSY_RX)
    {
      HAL_SPI_RxCpltCallback(hspi);
    }
    else if (State == HAL_SPI_STATE_BUSY_TX)
    {
      HAL_SPI_TxCpltCallback(hspi);
    }
	else
    {
      /* end of the appropriate call */
    }

When entering the IRQHandler, the "State" Variable is always "HAL_SPI_STATE_READY" therefore the callback functions are not called.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.