2019-09-01 11:43 AM
With the CubeMX 5.3.0 with the STM32G474RE V1.1.0 library is the assert_failed called when MX_DAC1_Init() is executed.
The DAC1 was configured as follow:
The assert was called from the "MX_DAC1_Init()" function
sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_AUTOMATIC;
sConfig.DAC_DMADoubleDataMode = DISABLE;
sConfig.DAC_SignedFormat = DISABLE;
sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
sConfig.DAC_Trigger2 = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_ENABLE; // <<====
sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)The sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_ENABLE is the cause called by
assert_param(IS_DAC_CHIP_CONNECTION(sConfig->DAC_ConnectOnChipPeripheral));The value for DAC_CHIPCONNECT_ENABLE is 6 but the macro "IS_DAC_CHIP_CONNECTION" tell is:
#define IS_DAC_CHIP_CONNECTION(CONNECT) (((CONNECT) == DAC_CHIPCONNECT_EXTERNAL) || \
((CONNECT) == DAC_CHIPCONNECT_INTERNAL) || \
((CONNECT) == DAC_CHIPCONNECT_BOTH))#if defined(STM32G4)
#define DAC_CHIPCONNECT_DISABLE (DAC_CHIPCONNECT_EXTERNAL | DAC_CHIPCONNECT_BOTH)
#define DAC_CHIPCONNECT_ENABLE (DAC_CHIPCONNECT_INTERNAL | DAC_CHIPCONNECT_BOTH)
#endifSo the "IS_DAC_CHIP_CONNECTION" has an incorrect definition, because it checks only for:
and for the DAC_CHIPCONNECT_ENABLE the macro must checks also the the combination of:
DAC_CHIPCONNECT_ENABLE (DAC_CHIPCONNECT_INTERNAL | DAC_CHIPCONNECT_BOTH)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.