2017-07-13 2:18 AM
I'd like to report a bug.
In the file usbh_hid_keybd.c, ver. V3.2.2, date: 07-July-2015
line 333:
Now is:
if(HID_Handle->length > (sizeof(keybd_report_data)/sizeof(uint32_t))){
HID_Handle->length = (sizeof(keybd_report_data)/sizeof(uint32_t)); }should be replaced with:
if(HID_Handle->length > sizeof(keybd_report_data)){
HID_Handle->length = sizeof(keybd_report_data); }If I did not make a change, the keyboard reported an error by sending a stall event.
Can anyone confirm this?
#host-usb-hid-keyboard2017-07-17 7:12 AM
Hi
Kania.Grzegorz.002
,Could you please precise the FW package you are using?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-07-18 2:18 AM
Hi Amel
I am using the STM32Cube_FW_F7_V1.3.0 package, but I found this file also in others, eg: STM32Cube_FW_F1_V1.4.0, STM32Cube_FW_F2_V1.6.0
Grzegorz
2017-12-21 3:09 PM
Well, I do have the same experience. A small keyboard I was planning to use (Gembird Mini Usb keyboard) stalled after ennumeration until I didn't change lines according KIania's recomendation. Thanks. Never the less the mentioned keyboard works in Linux without any problem as well as any other keyboard I tried with ST USB library. Strange.
I am using the last version
STM32Cube_FW_F7_V1.8.0.
Igor
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.