2017-09-27 10:03 AM
I want to turn on the led attached to PC.9. I do this:
LL_GPIO_InitTypeDef initStruct;
LL_GPIO_StructInit( &initStruct );
initStruct.Mode = LL_GPIO_MODE_OUTPUT_10MHz;
initStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
initStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
initStruct.Pin = LL_GPIO_PIN_9; // that equals 0x04020002
LL_GPIO_Init( GPIOC, &initStruct )
This code will actually init PC.2 (not PC.9 as it's supposed to) to output push-pull.
Why? LL_GPIO_Init does this:
pinpos = POSITION_VAL(GPIO_InitStruct->Pin);
where
&sharpdefine POSITION_VAL(VAL) (__CLZ(__RBIT(VAL)))
so pinpos will be equal to
(__CLZ(__RBIT(
0x04020002
))) which is equal to 1.Then current pin will be calculated like this:
currentpin = (GPIO_InitStruct->Pin) & (0x00000101U << pinpos);
so currentpint will be equal to 2.
And then
LL_GPIO_SetPinMode(GPIOx, currentpin, GPIO_InitStruct->Mode);
will be called, despite the fact that LL_GPIO_SetPinMode should only accept parameters like LL_GPIO_PIN_x.
Reasons:
I have already posted this bug here but it got mixed up with my own ignorance and stupidity so I haven't got a proper reaction. I believe it's time to post it again.
#hal-ll #ll-bug #software-error #bug #ll #stm32f1Solved! Go to Solution.
2018-03-27 3:51 AM
I'm glad that this issue is finally fixed but I'm startled that we still have to use community forum to submit issues about code. Moderators have to manually search for bugs and repost them in bug-tracker, users have to wait for several months just to be noticed!
Please, ST, please, make bug-tracker for code public! Or - better - make repository public (all of the code is open-source anyway, so why hide it?), a lot of the users will be glad to help with code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.