2019-11-11 1:25 PM
I am having a problem getting two DMA requests started for the same timer. One capture is an IC (input capture) and the other an OC (output compare). See the following code snippet
HAL_StatusTypeDef status;
status = HAL_TIM_OC_Start_DMA(&htim3,TIM_CHANNEL_1,(uint32_t *)TX_buf,TX_buf_len);
printf("Status TX: %u\r\n",status);
status = HAL_TIM_IC_Start_DMA(&htim3,TIM_CHANNEL_2,(uint32_t *)RX_buf,RX_buf_len);
printf("Status RX: %u\r\n",status);Both the OC and IC are working individually, but when I try to use both, whichever one is started second does not work. The first one always returns status 0 (HAL_OK). The second one always returns status 2 (HAL_BUSY). Both of these HAL API functions contain a check of htim->State. If I comment out the following in the function implementations, both calls work successfully
if (htim->State == HAL_TIM_STATE_BUSY)
{
return HAL_BUSY;
}
else if (htim->State == HAL_TIM_STATE_READY)
{
if ((pData == NULL) && (Length > 0U))
{
return HAL_ERROR;
}
else
{
htim->State = HAL_TIM_STATE_BUSY;
}
}
else
{
/* nothing to do */
}I believe the HAL library is incorrectly returning HAL_BUSY when starting the second DMA. My work around of commenting out code in the HAL library seems to work well. I would like a solution that doesn't require modifying the libraries.
I have verified the bug and the work around in "STM32Cube FW_G0 V1.3.0" and "STM32Cube FW_L0 V1.11.2"
2019-12-19 1:09 AM
Hello @JMano.2042 ,
Thank you for reporting this issue.
This is raised internally for fix in all impacted series.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.