2022-12-12 2:21 PM
The description for HAL_GetTickFreq says
/**
* @brief Return tick frequency.
* @retval tick period in Hz
*/
It returns 1 when the tick frequency is 1kHz. The period would be .001 seconds and the frequency would be 1000 Hz. Based on the typedef below, I'm not even sure what the units really are, but the description is clearly wrong.
typedef enum
{
HAL_TICK_FREQ_10HZ = 100U,
HAL_TICK_FREQ_100HZ = 10U,
HAL_TICK_FREQ_1KHZ = 1U,
HAL_TICK_FREQ_DEFAULT = HAL_TICK_FREQ_1KHZ
} HAL_TickFreqTypeDef;
Solved! Go to Solution.
2022-12-12 4:09 PM
It should be tick period in ms.
2022-12-12 4:09 PM
It should be tick period in ms.
2022-12-12 7:36 PM
Alas, the coder missed the intuitive and flexible way of coding a frequency.
2022-12-14 5:32 AM
Hello @MScha.8,
I confirm the issue and I reported internally.
Internal ticket number: 141253(This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-08 8:43 AM
Thank you Kaouthar.
It appears that both the enum and the function should be named something like TickPeriodInMilliseconds as suggested by Pavel A.
2023-01-08 11:57 AM
Maybe HAL_TICK_FREQ_nnnHZ can be memorized as HAL tick [period in ms] at frequency nnn HZ
2023-01-08 2:23 PM
period in HzThis one is a pure gold! Actually shows the level of understanding of the developers...
Also I wonder whether the designers stopped for a minute and looked around. There are reasons why every other system from small schedulers to large desktop OS counts ticks, not milliseconds!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.