2018-09-27 9:11 PM
Hi Team,
Recently, I came across an error "dereferencing pointer to incomplete type struct os_pool_cb " when in my program, I tried to access "markers" ( member of the struct os_pool_cb). Below is my design
file1.c
=======
#[include "cmsis_os.h"]
extern osPoolId mypool;
osPoolDef(rxDataPool, 16, sizeof(int));
mypool = osPoolCreate(osPool(rxDataPool));
if(mypool->markers) <=====(dereferencing pointer to incomplete type struct os_pool_cb)
file2.c
======
#[include "cmsis_os.h"]
osPoolId mypool;
uint32_t *ptr;
ptr = (uint32_t *)osPoolAlloc(mypool);
osPoolFree(mypool, ptr);
Solution
=========
Index: Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.c
===================================================================
--- Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.c (revision 4442)
+++ Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.c (working copy)
@@ -907,16 +907,6 @@
//This is a primitive and inefficient wrapper around the existing FreeRTOS memory management.^M
//A better implementation will have to modify heap_x.c!^M
^M
-^M
-typedef struct os_pool_cb {^M
- void *pool;^M
- uint8_t *markers;^M
- uint32_t pool_sz;^M
- uint32_t item_sz;^M
- uint32_t currentIndex;^M
-} os_pool_cb_t;^M
-^M
-^M
/**^M
* @brief Create and Initialize a memory pool^M
* @param pool_def memory pool definition referenced with \ref osPool.^M
Index: Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.h
===================================================================
--- Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.h (revision 4442)
+++ Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.h (working copy)
@@ -268,6 +268,16 @@
osTimerPeriodic = 1 ///< repeating timer^M
} os_timer_type;^M
^M
+typedef struct os_pool_cb {^M
+ void *pool;^M
+ uint8_t *markers;^M
+ uint32_t pool_sz;^M
+ uint32_t item_sz;^M
+ uint32_t currentIndex;^M
+} os_pool_cb_t;^M
Regards,
Manish
#cmsis #freertos-stm32cube #cubemx-v4.24
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.