2020-02-12 2:52 PM
2020-02-12 2:54 PM
For USBH_Start is USBH_LL_DriverVBUS (phost, TRUE) where
/**/**
* @brief Drive VBUS.
* @param phost: Host handle
* @param state : VBUS state
* This parameter can be one of the these values:
* 0 : VBUS Active
* 1 : VBUS Inactive
* @retval Status
*/
2020-08-09 4:09 PM
This issue still persists. Using H7 firmware version 1.8.0, for a Nucleo H743ZI
Quick Fix: Update the MX_DriverVbusFS function inside USB_HOST/Target/usbh_platform.c as follows (previously, the if-conditional was "state == 0"):
void MX_DriverVbusFS(uint8_t state)
{
uint8_t data = state;
/* USER CODE BEGIN PREPARE_GPIO_DATA_VBUS_FS */
if(state == 1)
{
/* Drive high Charge pump */
data = GPIO_PIN_SET;
}
else
{
/* Drive low Charge pump */
data = GPIO_PIN_RESET;
}
/* USER CODE END PREPARE_GPIO_DATA_VBUS_FS */
HAL_GPIO_WritePin(GPIOG,GPIO_PIN_6,(GPIO_PinState)data);
}ST, please provide a patch
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.