2022-08-09 11:44 PM
We are flashing the firmware to stm32g0b1ke mcu using i2c in-application programming.after flashing the firmware to mcu,changed the boot configuration to boot from flash memory.I set the boot pin to 0 and option bytes to 0xFAFFFEAA for booting from flash memory.
Setting the boot pin 0 not taking the firmware from flash memory.At this mode i cant access the mcu.changing the boot pin to 1 loading the system memory program.
whats the reason booting from flash memory not working?
2022-09-23 1:56 AM
Hello @VSoun.1,
I advise you checking the STM32 boot process FAQ. It might help you.
Thank you.
Chahinez
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.