cancel
Showing results for 
Search instead for 
Did you mean: 

bin file is gigantic, hex and elf files are normal, when defining a section of RAM in STM32F765VITx

BobbyBeta
Associate III

I'm trying to define a region of RAM for storing debug information that can persist following a reset (DEBUG_RAM). I'd like to put variables in a section (.debug_ram) that are stored in the DEBUG_RAM memory such its usage properly displays in the Build Analyzer.

When I do this my elf and hex files are a normal size, 1.3MB and 15kB respectively. My bin files, however, are 393MB. Unfortunately the company I work for has standardized on bin files, particularly for their bootloader software.

I have attached my modified linker file (renamed STM32F765VITX_FLASH.ld.c so that it can be attached to the forum) and main.c where I locate the debug_ram_test variable in the in the .debug_ram section. When I build the build analyzer window correctly shows that 6.25% of the DEBUG_RAM region is used.

If I use a bin-to-hex utility to convert the bin file I see it's almost all data records with all of the data equal to zero, interspersed with Extended Linear Address records outside the range for the FLASH for the MCU. Here is an example:

:10FFC000000000000000000000000000000000000000000000000000000000000000000031
:10FFD000000000000000000000000000000000000000000000000000000000000000000021
:10FFE000000000000000000000000000000000000000000000000000000000000000000011
:10FFF000000000000000000000000000000000000000000000000000000000000000000001
:01000004FF0FED
:100000000000000000000000000000000000000000000000000000000000000000000000F0
:100010000000000000000000000000000000000000000000000000000000000000000000E0
:100020000000000000000000000000000000000000000000000000000000000000000000D0
:100030000000000000000000000000000000000000000000000000000000000000000000C0 

I'm really hoping that I'm doing something dumb that I can fix, but I've done this on lots of projects before and probably never noticed because I only used hex files.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Could make DEBUG_RAM as a NOLOAD region if you don't want data initialization there.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

6 REPLIES 6
KnarfB
Super User

hex and elf formats can hold the bytes in several chunks or segments, bin cannot. Bin contains all the values between the lowest address and the highest. There is no way to change. Keep in mind, that even if your debug info persists after a (warm) reset, the content will be lost when the power goes down. Writing zeros to inbetween addresses might even cause side effects.

If the format really cannot be changed, you may add some startup code, actively copying the debug info from a global const (read-only) variable to the target adddess (or let a secondary bin file do so).

hth

KnarfB

The MCU only has 2MB of Flash so a 393MB bin file doesn't make sense. If I try to load the file in STM32CubeProgrammer it says that it's too big.

If I simply remove __attribute__((section(".debug_ram"))) from debug_ram_test in main.c, the bin file reduces to 6kB. It really shouldn't have an effect on the bin size where the variable is located in RAM but it does.

Long term I do plan on looking at the RCC->CSR register to determine the cause of reset before trusting the data in the .debug_ram section. I may use a CRC as well.

For now, however, I seem to get non-sensical bin files when I build with gcc and that's the first step.

Large because the file tries to put data from RAM into the BIN file, ie spanning 0x08000000 thru 0x20000080 (384MB). Binaries can't be sparse. Other tools would split to multiple binaries.

Stop putting data in RAM that needs to be staged in FLASH and moved there via code in startup.s

Check .MAP file, or dump .ELF object with objcopy

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Could make DEBUG_RAM as a NOLOAD region if you don't want data initialization there.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for writing me! I actually recognize your name from when I used to write here at my last job and I remember you being a really knowledgeable and helpful guy.

In my main.c I am not initializing the debug_ram_test variable so I wouldn't have expected it to store anything in FLASH that needs to be moved. In startup.s it just clears .bss and initializes .data but doesn't do anything to initialize my .debug_ram section (which is good as I want it to persistent between reboots).

I followed your advice to look at the map files, both with debug_ram_test in .debug_ram and then with debug_ram_test in .bss. Only 33 lines are different between the two, with debug_ram_test moving from .debug_ram to .bss and the other addresses shifting accordingly:

With debug_ram_test in .debug_ram:

.debug_ram      0x0000000020000000        0x8
                0x0000000020000000                . = ALIGN (0x4)
 *(.debug_ram)
 .debug_ram     0x0000000020000000        0x8 ./Src/main.o
                0x0000000020000000                debug_ram_test
                0x0000000020000008                . = ALIGN (0x4)
                0x0000000020000008                . = ALIGN (0x4)

.bss            0x000000002000008c       0x24
                0x000000002000008c                _sbss = .
                0x000000002000008c                __bss_start__ = _sbss
 *(.bss)
 .bss           0x000000002000008c       0x1c C:/ST/STM32CubeIDE_1.14.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/thumb/v7e-m+dp/hard/crtbegin.o
 *(.bss*)
 .bss.uwTick    0x00000000200000a8        0x4 ./Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.o
                0x00000000200000a8                uwTick
 .bss.linker_learn
                0x00000000200000ac        0x4 ./Src/main.o
                0x00000000200000ac                linker_learn
 *(COMMON)
                0x00000000200000b0                . = ALIGN (0x4)
                0x00000000200000b0                _ebss = .
                0x00000000200000b0                __bss_end__ = _ebss

._user_heap_stack
                0x00000000200000b0      0x600
                0x00000000200000b0                . = ALIGN (0x8)
                [!provide]                        PROVIDE (end = .)
                0x00000000200000b0                PROVIDE (_end = .)
                0x00000000200002b0                . = (. + _Min_Heap_Size)
 *fill*         0x00000000200000b0      0x200 
                0x00000000200006b0                . = (. + _Min_Stack_Size)
 *fill*         0x00000000200002b0      0x400 
                0x00000000200006b0                . = ALIGN (0x8)

With debug_ram_test in .bss:

.debug_ram      0x0000000020000000        0x0
                0x0000000020000000                . = ALIGN (0x4)
 *(.debug_ram)
                0x0000000020000000                . = ALIGN (0x4)
                0x0000000020000000                . = ALIGN (0x4)

.bss            0x0000000020000090       0x2c
                0x0000000020000090                _sbss = .
                0x0000000020000090                __bss_start__ = _sbss
 *(.bss)
 .bss           0x0000000020000090       0x1c C:/ST/STM32CubeIDE_1.14.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/thumb/v7e-m+dp/hard/crtbegin.o
 *(.bss*)
 .bss.uwTick    0x00000000200000ac        0x4 ./Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.o
                0x00000000200000ac                uwTick
 .bss.debug_ram_test
                0x00000000200000b0        0x8 ./Src/main.o
                0x00000000200000b0                debug_ram_test
 .bss.linker_learn
                0x00000000200000b8        0x4 ./Src/main.o
                0x00000000200000b8                linker_learn
 *(COMMON)
                0x00000000200000bc                . = ALIGN (0x4)
                0x00000000200000bc                _ebss = .
                0x00000000200000bc                __bss_end__ = _ebss

._user_heap_stack
                0x00000000200000bc      0x604
                0x00000000200000c0                . = ALIGN (0x8)
 *fill*         0x00000000200000bc        0x4 
                [!provide]                        PROVIDE (end = .)
                0x00000000200000c0                PROVIDE (_end = .)
                0x00000000200002c0                . = (. + _Min_Heap_Size)
 *fill*         0x00000000200000c0      0x200 
                0x00000000200006c0                . = (. + _Min_Stack_Size)
 *fill*         0x00000000200002c0      0x400 
                0x00000000200006c0                . = ALIGN (0x8)

I do suppose I'm surprised to see .bss start at 0x2000008c in the first map file and start at 0x20000090 in the second. I'd have expected them to both start at 0x20000080 as that's where RAM begins. I don't really see how these map file differences would cause the bin file corresponding to the first map file to be 393MB, however, and the bin file corresponding to the second map file to be 6kB.

NOLOAD seems to have worked!

With my debug variable in the DEBUG_RAM region I'm now getting a 6kB bin file!

Thank you so much for this!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.