2025-12-09 11:21 PM - last edited on 2025-12-10 3:50 AM by mƎALLEm
I am working on a NUCLEO-H753ZI board and want to set up Ethernet communication using LwIP in STM32CubeIDE.
I am looking for step-by-step guidance from the IOC file configuration to the generated code, including:
Pinout configuration for RMII (TX/RX, MDC/MDIO, REF_CLK)
LwIP middleware settings (heap size, pbuf pool, MEM_SIZE, etc.)
Memory layout for D2 SRAM / AXI SRAM for LwIP heap, DMA descriptors, RX/TX buffers
MPU region configuration for Ethernet and LwIP memory
Generating code and linker settings
Any tips to ensure that ping from PC works reliably
Could someone provide a complete, detailed guide or example project showing how to configure CubeIDE and LwIP for NUCLEO-H753ZI?
Solved! Go to Solution.
2025-12-10 3:49 AM - edited 2025-12-10 3:52 AM
Hello,
Please refer to this knowledge base article: How to create a project for STM32H7 with Ethernet and LwIP stack working (It seems it is using STM32H750-Discovery board).
2025-12-10 3:49 AM - edited 2025-12-10 3:52 AM
Hello,
Please refer to this knowledge base article: How to create a project for STM32H7 with Ethernet and LwIP stack working (It seems it is using STM32H750-Discovery board).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.