STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI and IIC bus not being free and locks up. Adding/removing code or changing stack size fixes the problem.

I have seen this with the SPI bus 6 months ago. It just just happened with the IIC bus. I am using Cube 1.12.0 and this maybe related to TKube.1 issue "Potential bug in I2C HAL layer (STM32Cube_FW_F4_V1.25.0) in I2C_MemoryTransmit_TXE_BTF() ?".I ha...

RobG by Associate III
  • 2108 Views
  • 3 replies
  • 0 kudos

Resolved! Does STM32CubeMX supports SafeRTOS?

It is well known that STM32Cube IDE & MX both has quiet good support for FreeRTOS, but my question is a bit different and related to SafeRTOS, I'm just wondering if ST has support for SafeRTOS as well or not?!I'm well aware that SafeRTOS comes with l...

JJ1 by Associate II
  • 2060 Views
  • 2 replies
  • 0 kudos

How can I send data over TCP / LwIp?

I am using Echoserver and EchoClient source code for stm32. I used `tcp_echoserver_init();` function to start callback and I tried to connect with python client to this server. And its successfully connect. I checked with wireshark. And python progra...

DCtech by Associate II
  • 1242 Views
  • 1 replies
  • 0 kudos

Resolved! STM32303E-EVAL

I bought the product, where can I get the basic firmware file for this product? I also want to see the basic code written in STMCUBEIDE. Thank you.

GKIM.11 by Associate
  • 1689 Views
  • 2 replies
  • 0 kudos

USB FS not sending correct amount of data

HelloI have been trying to debug an USB issue I've had on my STM32F722 Nucleo. For whatever input I try to send with CDC only two bytes are sent to my host PC. I'm using the latest HAL drivers.When breaking in the function USB_WritePacket() I can see...

Jaxc by Associate
  • 1114 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.