STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Built-in Bootloader

Hello everyone,I am working on an application about updating stm32f103 via built-in bootloader - uart.I have a bin file that is validated with cheksum equal to st-link utility tool. (sum all the bytes).My issue is that sometimes with the same bin fil...

TPrio.1 by Associate II
  • 3935 Views
  • 8 replies
  • 0 kudos

Resolved! SPI_DMATransmitCplt not checking the right address

Hi all,I'm working on a project that will communicate via SPI. I want to use DMA for it. I have some problem getting HAL_SPI_TxCpltCallback to be called. I've followed the debbuger and I think I've found what's wrong. It seems that the SPI_DMATransm...

0693W000007ZbyaQAC.png 0693W000007ZbyfQAC.png 0693W000007ZbykQAC.png 0693W000007ZcBKQA0.png

USB PD Audio Accessory connection

I am working with demo board B-G474E-DPOW1 and the project from the STM32CubeG4 Sink examples. I am trying to figure out how to connect an Audio Accessory. I have such an adapter. When I connect it to the usb-c, I expect to see an event with the conn...

ADoro.2 by Associate III
  • 3442 Views
  • 8 replies
  • 0 kudos

Optimization Settings for HAL Driver (STM32F7)

Hello,I have a project with FreeRTOS and LWIP (plus some other stuff). I ran into the problem, that if I set the optimization for my project (-O3 in my case) I get weird communication glitches. For example I only get a reply every 3rd or 4th ping, Pi...

H743ZI lwIP TCP assign more memory

Hello,I got the lwIP raw TCP working on my H743ZI2 NUCLEO which I'm quite proud of, but it's quite slow. Now I would like to assign more memory to the stack. By default it's running with 16KB heap I think. So the first thing I did was changing the MP...

MLang.7 by Associate III
  • 1732 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.