STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The difference between BOOT Loader and DFU mode??

I'm studying about the DFU mode to use this.​So I'm looking for documents, but I'm confused whether the DFU mode and BOOT Loader are different or the same.​I think,​There is ​various ways to communicate with the MCU in Boot Loader state like UART, I2...

JPark.20 by Associate II
  • 22843 Views
  • 2 replies
  • 0 kudos

Resolved! X-CUBE-AZRTOS-H7, how to use it?

I installed STM32CubeMX 6.2.0, the STM32CubeH7 1.9.0 and the X-CUBE-AZRTOS-H7 thinking that I would do Azure RTOS projects as I did using FreeRtos. Why didn't ST put Azure RTOS and its components as a midware option? As it does for FreeRtos.How to us...

Asantos by Senior
  • 1861 Views
  • 3 replies
  • 0 kudos

Resolved! Is there a FreeRTOS demo program for F4 or L4 ?

Is there a FreeRTOS demo program, using STM32CubeMX to set up, for:STM3240G-EVAL - EVAL with STM32F407IG MCU orSTM32L476G-EVAL with STM32L476ZGT6 orSTM32F429IDISCOVERY with STM32F429ZIT6Any help appreciated I want to use STM32CubeMX to set upany of t...

gerhard by Associate II
  • 1861 Views
  • 2 replies
  • 0 kudos

LWIP

I am having working tcp/ip project using lwip on STM32F7 using which I can send RAW data.Now I want to send text file from SD card to local server.How can I implement this.

Rohit.1 by Associate II
  • 3011 Views
  • 7 replies
  • 0 kudos

FreeRTOS contest switching time from ISR

Hi all,In my project I need to read an ADC at a sample rate of 15KSPS. When new data becomes ready to read, the ADC pull low the DRDY line. I've configured this line as input interrupt and in the ISR a signal is sent to a task waiting for it before t...

RCont.2 by Associate
  • 1177 Views
  • 1 replies
  • 0 kudos

I am wanting to create a USB audio device using the STM32 MCU. I am specifically wanting to connect multiple audio codecs. This needs to be a high quality audio device. I need some advice.

1) Is the STM32 capable of handling multiple audio codecs for audio transmission over USB?2) If so, what development boards would you recommend for getting familiar with it?3) Are there any tutorials for setup? Thanks!!!

BPalm.1 by Associate
  • 1122 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.