STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4P5 cannot connect to hTerm, "Error in OpenPort: Internal error when initializing 'COM4" or LabVIEW

Hello STM32-community,I'm struggling with the USB-connection via hTerm of my STM32. I'm trying to send a few bytes via USB, receiving them with the tool hTerm, but it cannot even connect to the Microcontroller. Terminal20141030 works just fine, whil...

0693W000008wD5CQAU.png
crackl1ng by Associate III
  • 1648 Views
  • 1 replies
  • 0 kudos

Resolved! Missing FLASH_CR_ERRIE in CMSIS of STM32F415xx

Hey,I'm programming with the STM32F415 MCU and discovered that the FLASH_CR_ERRIE declaration is missing in the CMSIS files. Is this a known issue or even intended?If it is not intended, I assume I can safely add the missing declaration? (I never had...

MGore by Associate
  • 1959 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.