STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32C092FCP6 FDCAN remapping issue.

I designed a board with a layout that I was very happy with, but this meant remapping FDCAN1_TX to PC14, which CubeMX dutifully created code for...However, the code wouldn't compile.  I needed to get my board order in that day so I simply adjusted th...

Resolved! USBX Audio Class frame done callback not called

I've set up my STM32U5A9J-DK to use ThreadX and connect to my PC via USBX and Audio Class.I'm correctly see the Audio Device on my PC and I can easily stream audio to it. The only thing is that, for some reason, the callback for new frame done is not...

nico23 by Senior III
  • 3000 Views
  • 22 replies
  • 3 kudos

Using STM32U5G-DK1 in USB OTG mode

Hello,I need to use STM32U5G-DK1 board in USB OTG mode. Right now with the help of examples provided by STM for STM32U5G-DK1 and DK2 board, I am able to use DK1 either in Device mode or in Host mode. In order to use it in OTG mode what changes need t...

Resolved! SDMMC + STM32H723 not initializing SD Card

I am having difficulties with initializing a SD Card.I am making use of the generated code to initialize the card:void MX_SDMMC1_SD_Init(void) I measured with a scope and I am getting 400KHz clock. All the pull-up resistors are correct and voltage is...

diktril by Associate III
  • 179 Views
  • 2 replies
  • 0 kudos

Resolved! STM32N6570-DK NonSecure Application not run.

Hi,I am creating a project CubeMX that uses both Secure and NonSecure.I using USART1 for debugging, and my application only runs on SecureApp and cannot run NonSecureApp. I tried implementing the same as Template Isolation XIP but it still didn't wor...

TrungDT by Associate
  • 134 Views
  • 1 replies
  • 0 kudos

STM32H7 Firmware Update - No Ping

Hello ST Community, I've recently updated the firmware for my project to the latest release in CubeMX V6.17.0I'm using the STM32H743XIH6 device... and the firmware pack was updated to STM32Cube MCU Package for STM32H7 version 1.13.0When I create a ne...

Resolved! Wakeup from standby with RTC on STM32C5

Hello,   I am using the RTC wakeup from the power standby example provided in the STM32C5 repository. The example starts the RTC wake-up timer and places the device in standby mode. The device does go to standby, and it does wake up due to the RTC wa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.