STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f103c8 canbus problem

stm32f103c8 canbus problemstm32cube version 6.2.1hal version 1.8.3when i want to send data from can bus, , it doesn't work when usart global interrupt is not on, is this error? Is it normal, I couldn't understandusart1 global interrupt=enabled >> w...

HKiri.1 by Associate
  • 728 Views
  • 0 replies
  • 0 kudos

Resolved! I have a project using STM32H745 processor that has network connectivity. All works awesome until the processor temp reaches about 120 F, then I start to lose connectivity. I am using RMII interface and again works perfectly at high bandwidth when < 120F

What could be the cause. I have checked the power circuitry. The rest of application still functions well. DMA, Timers, SPI, etc. Just network data is stalled. When temp goes down it resumes.

DPitt.1 by Associate II
  • 7026 Views
  • 17 replies
  • 0 kudos

H743ZI2 SDMMC with DMA (MDMA)

Hi, I've been trying to use SDMMC1 on the h743ZI2 nucleo board but can't get it to work with (M)DMA (it works without DMA with straight HAL code) as I always get HAL_SD_ERROR_TX_UNDERRUN when trying to format the card.I have copied the rtos threads f...

OHaza.1 by Associate III
  • 2484 Views
  • 5 replies
  • 1 kudos

Resolved! How to configure DFU from Cube MX

Hi to all,I want to configure DFU to create a USB bootloader for STM32F401RE (I need to understand it on this hardware for future implementation on different MCU). I have some questions.I configure CubeMX as the .ioc file attached.The main settings a...

ABatt.1 by Senior
  • 2861 Views
  • 4 replies
  • 0 kudos

LWIP on STM32H7 and Cubemx not working

I am using STM32H7 MCU and Cubemx ide. I am facing an issue with ethernet connectivity with the Nucleo board which has STM32H743 mcu.I have configured Connectivity ETH and set the mode to RMII and enabled LWIP from the middleware. I tried DHCP enable...

SS.Sagar by Associate III
  • 2421 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.