STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the correct systemClock_Config to use in order to have USB OTG FS with a 48MHz external cristal as the clock source ?

Hi, I am working with a STM32H743 and I am trying to use USB OTG FS with the best clock configuration possible. I would like to have a SYSCLK at 480MHz and use the USB OTG FS with the external clock source HSE at 48MHz.The frequency of the external c...

ALE C.1 by Associate II
  • 5490 Views
  • 6 replies
  • 0 kudos

USB HS and FS Pin Mapping issue.

Hello,I am working on STM32H745IIK controller.I am enabling the FS and HS USB configuration.This is very Important connection ,the USB HS is used for accessing the data come from the PC application and the data comes in veryhigh speed.FS mode is use...

0693W00000HqH0ZQAV.png 0693W00000HqGzmQAF.png
MDeva.1 by Associate II
  • 1052 Views
  • 0 replies
  • 0 kudos

Resolved! HAL Librarys Return Values

Hello Everyone. I'm a student and learning ST nowadays.Forgive me for my childish question but I really don't get it.HAL library's functions are usually returns a value of result of the process.For example, HAL_Init func returns HAL_StatusTypeDef val...

Amewp.1 by Associate II
  • 3957 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.