STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi all, I enabled USB on 407 controller in MS Class and through program I am enabling (MX_USB_DEVICE_Init();) and disabling (MX_USB_DEVICE_DeInit ();) it. Once enabled, it looks as though the controller gets stuck in a loop. It does not execute

other functions and just hangs. I am suspecting some interrupt flag not being cleared. Strangely it works on my laptop but not on a PC. An earlier version is working without getting stuck and shows SD card content. Any suggestions please?

X-CUBE-USB-AUDIO Sychronization Characteristic

Hello together,i'm using the X-CUDE-USB-AUDIO expansion pack with the Development Board STM32F769 Discovery Kit. We plan to integrate it later on into our product. The example project for playback and recording works fine. But we wonder which synchro...

ESawa.1 by Senior
  • 994 Views
  • 0 replies
  • 0 kudos

Resolved! netconn_connect() for TCP/IP connection is blocking at osSemaphoreAcquire(TxPktSemaphore,...) on my STM32F746ZG-Nucleo

I try to implement a TCP/IP client on my STM32F746ZG-Nucleo.Before the last update it was working. But no more now.The first pass I always get a ERR_RTE because the ethernet link is not up. So I tried to connect each 5 secondes 5 times.But the second...

Resolved! Example of MEMS microphone and PDM 2 PCM on STM32

Hello,I am hoping to find someone who could explain or show an example of how to read data line from a MEMS microphone using PDM and output the corresponding PCM values. If anyone could help with some code examples I would be very much appreciative....

kcire L. by Associate III
  • 6109 Views
  • 3 replies
  • 0 kudos

MQTT: authentication error in server side

Hi, I am new to MQTT and LWIP.I am trying to implement MQTT client in STM32F407 and to connect to MQTT server through LWIP.When I tried connecting to MQTT server, I received authentication error in server side.Kindly help resolve the issue. mqtt_clie...

TG.3 by Associate II
  • 2742 Views
  • 1 replies
  • 0 kudos

ADC sporadic fails when USB communication

I am working on a new PCB/platform based on the STM32H730 MCU.In general, all peripheral drivers work well, using Cube MX.But I have a problem with the ADC sampling:I quite often see errors on the ADC sampling, when USB is connected to PC.But only wh...

KKjel.1 by Senior
  • 1250 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.