STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

REAL TIME CLOCK (RTC) Not working correctly.

Using HAL library set up RTC, but at times SKIPS seconds. WHY?This is the setup:static void MX_RTC_Init(void){ /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ RTC_TimeTypeDef sTime = {0}; RTC_DateTypeDef sDate = {0}; /* USER CODE BEGI...

GSalz.1 by Associate II
  • 2952 Views
  • 4 replies
  • 0 kudos

Resolved! Trace Hook Macros in Azure RTOS ThreadX

Hello,I worked until now with FreeRTOS. And in FreeRTOS there are Trace Hook Macros.Is there an equivalent on Azure RTOS ThreadX?Trace hook macros on FreeRTOS are a very powerful feature that permit you to collect data on how your embedded applicatio...

MStew.1 by Associate III
  • 2404 Views
  • 2 replies
  • 1 kudos

Resolved! HAL_UART functions do not work with Azure RTOS ThreadX

Hello,I followed this guide:https://community.st.com/s/article/how-does-the-threadx-semaphore-workAnd everything works.But when I try to add a modification, a HAL_UART_Transmit - HAL_UART_Transmit(&huart2, (uint8_t *)&message, 1, 10); - in one thread...

MStew.1 by Associate III
  • 4296 Views
  • 6 replies
  • 0 kudos

Resolved! Question about the Azure RTOS ThreadX Semaphore example

Hello,in the Semaphore example(https://community.st.com/s/article/how-does-the-threadx-semaphore-work) there is this step:Open Core\Src \main.c – you can copy and paste the code below, but please notice the" USER CODE BEGIN", to properly place the co...

MStew.1 by Associate III
  • 2729 Views
  • 3 replies
  • 0 kudos

Driver for ksz8863 switch?

Hi, does ST have it's own driver implementation of the ksz8863 switch. If yes where can i download it. I like to have an link up/down feedback. Need to have connection to the internal register of that switch. For now i just use the lan8742 driver pro...

MOtto.2 by Associate II
  • 5932 Views
  • 4 replies
  • 1 kudos

Resolved! custom bootloader problem on STM32F405

helloi am working on a custom bootloader or STM32F405.the Flash process is done correctly by the Bootloader, i checked the content of the flash.the problem happens when the bootloader jumps to the application firmware which is located at adress 0x080...

0693W00000aHet4QAC.jpg 0693W00000aHetPQAS.jpg
ZTale.1 by Associate II
  • 5914 Views
  • 10 replies
  • 0 kudos

Resolved! SDCard (SDIO) connector on stm32f723e-disco

Hi all,is it possible to connect a SDCard to the stm32f723e-disco [1] board? The webpage [1] is talking about some microSD connector, but I do not really find one. So is this a mistake on the webpage?Additionally, I would like to ask, if it is possib...

whati001 by Associate II
  • 1577 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H725 supports VCP over USB?

Hello,i am porting a project made initially on STM32H750, but because of the semiconductor shortage on the market, the only available part was a stm32H725IGK6, which i started working on.Regarding the usb connection, i have the following pins used:P...

Bogdan by Senior
  • 2210 Views
  • 3 replies
  • 0 kudos

How do i use HAL_UART in AZURE RTOS

Hi i would like to have an example code or something that helps me out, I wanna know how to use HAL functions in AZURE RTOS ,When i try to use HAL_UART_TRANSMIT(&huart2,pdata,size,timeout) i get an error that huart is not defined like wise same for P...

SC.J.1 by Associate
  • 1582 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.