STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware update over OTA for stm32g491RE

Hi,I am working with stm32g491re.I need to give firmware update option to the mcu . My stm32 board connected other MCU through uart and other mcu connected to web server. Firmware updates will come from webserver to stm32 through other mcu(with UART)...

stm32h750 lwip mqtt hardfault issues

Dear Technical team,We are developing an IoT product using STM32H750.The application starts a task cycle to publish customer information to the cloud platform by MQTT Publish API.At the same time, we make a ping tests to target board from the PC host...

martin_xu by Associate II
  • 1469 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H747 I2S slave mode

Hello, I have a setup where I use an STM32H747XIH6U and an ADAU1361 codec on the I2S-interface. I want to use the PDM-mics on the ADAU, and in order to do that, ADAU has to be in I2S master mode according to the datasheet. Consequently, STM has to be...

lukasma by Associate III
  • 9254 Views
  • 15 replies
  • 1 kudos

Resolved! Help needed with STM32 ASM function

Hallo All,I am currently stuck and need your help. The following function counts the no. of 1 in a 32 bit word on an STM32F407. Why does it fail for values which have their bit 31 set? Precisely, it ignores bit 31 and in these cases is off by one. ...

herbert by Associate III
  • 3211 Views
  • 4 replies
  • 6 kudos

Resolved! Issues with I2C Direction Changes

Hello;I am working with STM32CubeIDE, trying to connect a Nucleo-L4R5ZI board to an ADCS chip using I2C. The method of communication is very strange, requiring: [start condition] - [controller sends two bytes] - [start condition] - [controller sends ...

DeemDeem52_0-1710289722807.png DeemDeem52_1-1710289820964.png

STM32H743XI DAC1 / DAC OP Value change after some time.

CONFIGURATION:USING STM32H743XI DAC1 / DAC OP: CONFIGURATION: NORMAL BUFFERED OUTPUT MODE.PINNO: PA4 & PA5. using HAL_DAC_SetValue function to change DAC values - 0 to 3.0 V. if want to set 2.0 V, respective cnt applied using HAL_DAC_SetValue, at DAC...

Ab1 by Associate II
  • 1229 Views
  • 1 replies
  • 0 kudos

XMODEM protocol for file transfer

Hi,I'm currently working on file transfer through the XMODEM protocol, and I want to implement the logic in STM32CubeIDE. If anyone has already implemented it, please share the source code. It would be helpful for me. Thanks

pvall.1 by Associate II
  • 18096 Views
  • 15 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.